Migrate prj from S32DS for ARM version2018.R1 TO S32 platform 3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Migrate prj from S32DS for ARM version2018.R1 TO S32 platform 3.4

Jump to solution
3,861 Views
oceansea
Contributor III

ZWMO$S1%J_[LHL926EJMCIM.png

hi,

i want Migrate prj from S32DS for ARM version2018.R1 TO S32 platform 3.4

i do this:

  1. Click File > Import... > General > Existing Projects into Workspace, then click Next.
  2. Click Browse... and browse to the project location, click OK, select the Copy projects into workspace option, then click Finish.
  3. i  click migrate it show the picture,have no prj;

it confuse me,how migrate prj.

thanks!

Labels (2)
0 Kudos
Reply
1 Solution
3,848 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2

S32K1xx development package and S32SDK S32K1XX RTM 4.0.2 need to be installed.

S32K1xx development package S32SDK S32K1XX RTM 4.0.2.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
3,849 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2

S32K1xx development package and S32SDK S32K1XX RTM 4.0.2 need to be installed.

S32K1xx development package S32SDK S32K1XX RTM 4.0.2.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,842 Views
oceansea
Contributor III

oceansea_0-1680160552410.png

hi,

i haven installed the S32K1XX development package ,but the IDE only have S32SDK S32K1XX RTM 4.0.3,not 

S32SDK S32K1XX RTM 4.0.2

 

0 Kudos
Reply
3,838 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please install S32 SDK for S32K1xx RTM 4.0.2 offline.(S32 Design Studio v3.4 S32K1 Service Pack 1 released!)

0 Kudos
Reply
3,830 Views
oceansea
Contributor III

hi,

now i installed S32K1XX deveiopment package and S32SDK S32K1XX RTM 4.0.2

oceansea_0-1680164829252.png

oceansea_1-1680164880064.png

 

 

but when i click migrate ,it still have nothing;

oceansea_2-1680164913369.png

thanks

0 Kudos
Reply
3,810 Views
mikedoidge
NXP Employee
NXP Employee

Have you tried to verify your setup by repeating the process for the project shown in the video? ammclib_s32K116

If it works for this project, then you know the setup is correct. The issue then must be related to the project you are trying to convert.

Best Regards,

Mike

0 Kudos
Reply