Migrate prj from S32DS for ARM version2018.R1 TO S32 platform 3.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Migrate prj from S32DS for ARM version2018.R1 TO S32 platform 3.4

跳至解决方案
3,825 次查看
oceansea
Contributor III

ZWMO$S1%J_[LHL926EJMCIM.png

hi,

i want Migrate prj from S32DS for ARM version2018.R1 TO S32 platform 3.4

i do this:

  1. Click File > Import... > General > Existing Projects into Workspace, then click Next.
  2. Click Browse... and browse to the project location, click OK, select the Copy projects into workspace option, then click Finish.
  3. i  click migrate it show the picture,have no prj;

it confuse me,how migrate prj.

thanks!

标签 (2)
0 项奖励
回复
1 解答
3,812 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2

S32K1xx development package and S32SDK S32K1XX RTM 4.0.2 need to be installed.

S32K1xx development package S32SDK S32K1XX RTM 4.0.2.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,813 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2

S32K1xx development package and S32SDK S32K1XX RTM 4.0.2 need to be installed.

S32K1xx development package S32SDK S32K1XX RTM 4.0.2.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,806 次查看
oceansea
Contributor III

oceansea_0-1680160552410.png

hi,

i haven installed the S32K1XX development package ,but the IDE only have S32SDK S32K1XX RTM 4.0.3,not 

S32SDK S32K1XX RTM 4.0.2

 

0 项奖励
回复
3,802 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please install S32 SDK for S32K1xx RTM 4.0.2 offline.(S32 Design Studio v3.4 S32K1 Service Pack 1 released!)

0 项奖励
回复
3,794 次查看
oceansea
Contributor III

hi,

now i installed S32K1XX deveiopment package and S32SDK S32K1XX RTM 4.0.2

oceansea_0-1680164829252.png

oceansea_1-1680164880064.png

 

 

but when i click migrate ,it still have nothing;

oceansea_2-1680164913369.png

thanks

0 项奖励
回复
3,774 次查看
mikedoidge
NXP Employee
NXP Employee

Have you tried to verify your setup by repeating the process for the project shown in the video? ammclib_s32K116

If it works for this project, then you know the setup is correct. The issue then must be related to the project you are trying to convert.

Best Regards,

Mike

0 项奖励
回复