Generated files are referring headers from SDK in installing folder.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Generated files are referring headers from SDK in installing folder.

跳至解决方案
2,076 次查看
tejo2one
Contributor III

I am using MPC5748G development kit with S32DS., new project is created by selecting create from example the generated files are referring header files from installing folder instead of project folder.

Any changes made to project folder are not being reflected to project instead header files in installing location are being reflected to project.

As a work around header included as following:

tejo2one_0-1677739401547.png

 

Please let me know if there is permanent solution.

 

0 项奖励
回复
1 解答
2,025 次查看
tejo2one
Contributor III

Thanks for response. I did little search and found it.

.PE file already contained generate mode as "standalone".

I just removed include paths which were pointing to "c-drive" in "properties/Paths and Symbols/Includes".

After update:

tejo2one_0-1678117791185.png

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,034 次查看
Markus_Schroeder
Contributor II

I found the updated link:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-SDK-based-example-code-as-st...

Actually, it seems, the link was correct, only the 4 at the end was not interpreted as part of it.

0 项奖励
回复
2,026 次查看
tejo2one
Contributor III

Thanks for response. I did little search and found it.

.PE file already contained generate mode as "standalone".

I just removed include paths which were pointing to "c-drive" in "properties/Paths and Symbols/Includes".

After update:

tejo2one_0-1678117791185.png

 

0 项奖励
回复
2,057 次查看
jiri_kral
NXP Employee
NXP Employee
0 项奖励
回复
2,046 次查看
tejo2one
Contributor III

Thanks for response, page is no longer available.

Can you please check & reshare?

tejo2one_0-1678011623989.png

 

0 项奖励
回复