Generated files are referring headers from SDK in installing folder.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generated files are referring headers from SDK in installing folder.

Jump to solution
2,120 Views
tejo2one
Contributor III

I am using MPC5748G development kit with S32DS., new project is created by selecting create from example the generated files are referring header files from installing folder instead of project folder.

Any changes made to project folder are not being reflected to project instead header files in installing location are being reflected to project.

As a work around header included as following:

tejo2one_0-1677739401547.png

 

Please let me know if there is permanent solution.

 

0 Kudos
Reply
1 Solution
2,069 Views
tejo2one
Contributor III

Thanks for response. I did little search and found it.

.PE file already contained generate mode as "standalone".

I just removed include paths which were pointing to "c-drive" in "properties/Paths and Symbols/Includes".

After update:

tejo2one_0-1678117791185.png

 

View solution in original post

0 Kudos
Reply
4 Replies
2,078 Views
Markus_Schroeder
Contributor II

I found the updated link:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-SDK-based-example-code-as-st...

Actually, it seems, the link was correct, only the 4 at the end was not interpreted as part of it.

0 Kudos
Reply
2,070 Views
tejo2one
Contributor III

Thanks for response. I did little search and found it.

.PE file already contained generate mode as "standalone".

I just removed include paths which were pointing to "c-drive" in "properties/Paths and Symbols/Includes".

After update:

tejo2one_0-1678117791185.png

 

0 Kudos
Reply
2,101 Views
jiri_kral
NXP Employee
NXP Employee
0 Kudos
Reply
2,090 Views
tejo2one
Contributor III

Thanks for response, page is no longer available.

Can you please check & reshare?

tejo2one_0-1678011623989.png

 

0 Kudos
Reply