CSEc:Description of user keys in S32KRM and AN5401

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSEc:Description of user keys in S32KRM and AN5401

Jump to solution
1,111 Views
ZEROOO
Contributor IV

Hi

    Why does the S32k manual say that the number of user keys is 20 and that of AN5401 is 17? How should we interpret these two tables?

S32 RM:

ZEROOO_0-1692694715734.png

 

AN5401:

ZEROOO_1-1692694731460.png

ZEROOO_2-1692694753998.png

 

 

 

0 Kudos
Reply
1 Solution
1,091 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ZEROOO 

There are two sections about flash memory - one for the FTFC module and the second for the FTFM module.

The FTFC flash is on all S32K1 devices except S32K14xW. So, FTFM is on S32K14xW only. This one was designed later for an extended temperature range.
If you check the FTFC description (Cryptographic Services Engine (CSEc) module features section), you can find: "Secure cryptographic key storage (ranging from 3 to 17 user keys)".

If you check the FTFM description: "Secure cryptographic key storage (up to 20 user keys)".

AN5401 was written before the launch of S32K14xW, so it's not mentioned there. So this is just not up to date in this matter.

 

B.R.

VaneB

View solution in original post

1 Reply
1,092 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ZEROOO 

There are two sections about flash memory - one for the FTFC module and the second for the FTFM module.

The FTFC flash is on all S32K1 devices except S32K14xW. So, FTFM is on S32K14xW only. This one was designed later for an extended temperature range.
If you check the FTFC description (Cryptographic Services Engine (CSEc) module features section), you can find: "Secure cryptographic key storage (ranging from 3 to 17 user keys)".

If you check the FTFM description: "Secure cryptographic key storage (up to 20 user keys)".

AN5401 was written before the launch of S32K14xW, so it's not mentioned there. So this is just not up to date in this matter.

 

B.R.

VaneB