CSEc:Description of user keys in S32KRM and AN5401

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CSEc:Description of user keys in S32KRM and AN5401

跳至解决方案
1,110 次查看
ZEROOO
Contributor IV

Hi

    Why does the S32k manual say that the number of user keys is 20 and that of AN5401 is 17? How should we interpret these two tables?

S32 RM:

ZEROOO_0-1692694715734.png

 

AN5401:

ZEROOO_1-1692694731460.png

ZEROOO_2-1692694753998.png

 

 

 

0 项奖励
回复
1 解答
1,090 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @ZEROOO 

There are two sections about flash memory - one for the FTFC module and the second for the FTFM module.

The FTFC flash is on all S32K1 devices except S32K14xW. So, FTFM is on S32K14xW only. This one was designed later for an extended temperature range.
If you check the FTFC description (Cryptographic Services Engine (CSEc) module features section), you can find: "Secure cryptographic key storage (ranging from 3 to 17 user keys)".

If you check the FTFM description: "Secure cryptographic key storage (up to 20 user keys)".

AN5401 was written before the launch of S32K14xW, so it's not mentioned there. So this is just not up to date in this matter.

 

B.R.

VaneB

在原帖中查看解决方案

1 回复
1,091 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @ZEROOO 

There are two sections about flash memory - one for the FTFC module and the second for the FTFM module.

The FTFC flash is on all S32K1 devices except S32K14xW. So, FTFM is on S32K14xW only. This one was designed later for an extended temperature range.
If you check the FTFC description (Cryptographic Services Engine (CSEc) module features section), you can find: "Secure cryptographic key storage (ranging from 3 to 17 user keys)".

If you check the FTFM description: "Secure cryptographic key storage (up to 20 user keys)".

AN5401 was written before the launch of S32K14xW, so it's not mentioned there. So this is just not up to date in this matter.

 

B.R.

VaneB