S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe 2. Download and Install S32 Design Studio 3.5 Update 2 D2302: SW32_S32DS_3.5.2_D2302.zip  (com.nxp.s32ds.update_3.5.2.20230227110156)   3. Download and Install S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices(3.5.0_D2303): SW32K3xx_S32DS_3.5.0_D2303.zip  (com.nxp.s32ds.sp1.s32k3xx.update_3.5.0.20230405175452)   4. For users who need to install S32K396 RTD for development, please download and install S32 Design Studio Service Pack 1 RTM with support for S32K39x devices(3.5.0_D2303): SW32K39x_S32DS_3.5.0_D2303.zip (com.nxp.s32ds.sp1.s32k396.update_3.5.0.20230330)   5.a) For users who need to install S32M276 RTD in S32K3 RTD 3.0.0\P01\P01 HF01\P01 HF02 for development, please download and install S32 Design Studio Service Pack 2 CD with support for S32M2xx devices (3.5.0_D2302😞 SW32M2xx_S32DS_3.5.0_D2302.zip(com.nxp.s32ds.s32m2.update_3.5.0.20230222151347)  Note: Please contact your local FAE to enable for you download the S32M276 development package. 5.b) For users who need to install S32M276 RTD in S32K3 RTD 3.0.0 P07 for development, , please download and install S32 Design Studio Service Pack 2 EAR2 with support for S32M2xx devices(3.5.0_D2303😞 SW32M2xx_S32DS_3.5.0_D2303.zip(com.nxp.s32ds.s32m2.update_3.5.0.20230328160305)   6. Select and install one of the following updatesite for S32K3 RTD 3.0.0: 6.a) Download and install S32K3 Real-Time Drivers Version 3.0.0: SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip   6.b) Download and install S32K3 Real-Time Drivers Version 3.0.0 P01 : SW32K3_RTD_4.4_3.0.0_P01_D2303_DS_updatesite.zip   6.c) Download and install S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 (3.0.0_P01_HF02😞 SW32K3_RTD_4.4_3.0.0_P01_HF02_DS_updatesite_D2305.zip   6.d) Download and install S32K3_M27X Real-Time Drivers Version 3.0.0 P07: SW32K3_RTD_R21-11_3.0.0 _P07_D2307.zip  
View full article
The S32K3 RTD 2.0.0 lacks SIUL2 external interrupt function. Siul2_Icu is part of Icu(Input Capture Unit), the main function of the example should have been: use the Icu and Dio drivers to toggle a LED on a push button. But it doesn't. So this document will show the step-by-step process to add 'SIUL2 external interrupt' function in Siul2_Port_Ip_Example_S32K344 using the S32K3xx RTD LLD(Low Level Driver) and the S32 Configuration Tools. This example is for the S32K3X4EVB-Q257, connected to a PC through USB (OpenSDA) connection. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32K1xx development package and the S32K1 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. Launch S32 Design Studio for S32 Platform Procedure 1. Import Siul2_Port_Ip_Example_S32K344 example File->New->S32DS Project from Example It can be seen that in the Icu (Input Capture Unit Driver) folder of S32K3 RTD 2.0.0, there are only interrupt routines implemented by the Emios module for the time being, and external interrupt routines for the EIRQ pin of the Siul2 module does not exist. Here we import the Siul2_Port_Ip_Example_S32K344 routine, and add the Siul2_Icu part on this basis.   2. Add push button and LED in Pins tool Add the pins for user buttons (SW4 PTB26 SIUL2 eirq13) according to the S32K3X4EVB-Q257.   3. Add IntCtrl_Ip component Go to Peripherals tool. Here we can see that the ‘Siul2_Dio’ and ‘Siul2_Port’ components are already added. From the Components view, click on ‘Add a new configuration component…’ button from the Drivers category. This will bring up a list of non-AUTOSAR components. Locate and then select the ‘IntCtrl_Ip’ component from the list and click OK. Option 1: Keep the default setting after add ‘IntCtrl_Ip’ component(Here we didn't change the settings of ‘IntCtrl_Ip’, nor use IntCtrl_Ip_Init and IntCtrl_Ip_ConfigIrqRouting API to enable interrupts and install handlers in IntCtrl_Ip).This routine only uses one interrupt, so we will call IntCtrl_Ip_InstallHandler and IntCtrl_Ip_EnableIrq those two APIs to install and enable the SIUL2 EIRQ13 IRQ separately. Option 2: User can enable many interrupts in the Interrupt Controller configuration(Note user can only add one interrupt controller configuration in the RTD); Meanwhile, it can set interrupt’s priority separately. The two APIs IntCtrl_Ip_Init and IntCtrl_Ip_ConfigIrqRouting can initialize these interrupts as a whole. The name of the Handler in the Generic Interrupt Settings tab needs to be the same as the name in peripheral_Ip_Irq.c of the corresponding peripheral. For example, this routine uses the PTB26 SIUL2 EIRQ13 external interrupt, which can be found in RTD/src/Siul2_Icu_Ip_Irq.c: ISR(SIUL2_EXT_IRQ_8_15_ISR) According to the "Table 35" of S32K3XXRM reference manual, we can see the SIUL2 EIRQ13(PTB26) external interrupt used in this routine belongs to SIUL_1_IRQn and the Handler name SIUL2_EXT_IRQ_8_15_ISR.   4. Add Siul2_Icu component Click on ‘Add a new configuration component…’ button from the Drivers category. Locate and then select the ‘Siul2_Icu’ component from the list and click OK. Step 5 select SIUL2_0_IRQ_CH_13 because this routine selects the onboard SW4 PTB26 SIUL2 EIRQ13 external interrupt (the onboard SW5 PTB19 pin has no EIRQ external interrupt function, so I did not added here). Step 6 set DIRER0[EIREn] to enable this external interrupt pin. Step 8 set the IFCPR[IFCP] filter clock prescaler. Step 10 input 13 for the Hardware channel due to we use SIUL2 EIRQ13. Step 11 set IFER0[IFEn] to enable the glitch filter for the external interrupt pin. Step 12 set IFMCRn[MAXCNT] to assign value to the external interrupt filter counter. Step 14 select the IcuSiu2Channel_0 channel configured in the IcuSiul2 tab above. Step 15 select the ICU_RISING_EDGE according to the SW4 button circuit (press to generate a rising edge). Step 16 Because the SIUL2 EIRQ external interrupt is used in this routine, ICU_MODE_SIGNAL_EDGE_DETECT mode must be selected. Step 17 add the corresponding callback function name. That is, it corresponds to the notification after the SIUL2 EIRQ external interrupt pin captures the rising edge (the interrupt flag does not need to be cleared here, the driver has already been implemented it).   5. Include the headers for the drivers used in the application #include "Siul2_Icu_Ip.h" #include "IntCtrl_Ip.h"   6. Add Siul2_Icu LLD APIs Siul2_Icu_Ip_Init is used to initialize all Siul2_Icu channels generated by the S32 Configuration Tools (this routine only configures the channel SW4 PTB26 SIUL2 EIRQ13). Siul2_Icu_Ip_EnableInterrupt enable Siul2 IRQ interrupt for the specified channels. Siul2_Icu_Ip_EnableNotification enable callback function of Siul2 IRQ interrupt for the specified channels. This routine uses the SW4 button to trigger the PTB26 SIUL2 EIRQ13 external interrupt callback function SW4_eirq13_PTB26_Callback to flip the PTB18 D33 red LED.   7. Add IntCtrl LLD APIs IntCtrl_Ip_InstallHandler installs the SIUL2_EXT_IRQ_8_15_ISR interrupt handler generated by the S32 Configuration Tools. IntCtrl_Ip_EnableIrq enables the corresponding interrupt. Why input SIUL_1_IRQn and SIUL2_EXT_IRQ_8_15_ISR has been explained at the end of "4. Adding the IntCtrl_Ip component" above. References - S32K3xx Pins and Clocks with RTD - Training - AN13435: SDK/MCAL to Real-Time Drivers - Integration Manual for S32K3 ICU Driver (RTD_ICU_IM.pdf) - User Manual for S32K3 ICU Driver (RTD_ICU_UM.pdf) - Integration Manual for S32K3 PLATFORM Driver (RTD_PLATFORM_IM.pdf) - User Manual for S32K3 PLATFORM Driver (RTD_PLATFORM_UM.pdf)
View full article
Quick Fix is a feature of the Java editor in Eclipse which enables a user to resolve problems found in the Java code of their project. This feature is available to be used within S32 Design Studio for some problems. Such problems will be identified with the 'light bulb' icon in the description field, as shown below: For example, such problems sometimes occur when importing a project created in a previous version of S32 Design Studio, are provided from another user, or some files in a project have become corrupted. To resolve issues identified with the 'light bulb' icon, right-click on the problem and from the pop-up menu, select 'Quick Fix'.  The Quick Fix menu will appear, providing the available solutions for the problem. In most cases, there will be just one solution. Click finish to implement the fix. In some cases, more information will be required from the user to complete the fix. Complete the form to provide the additional information, then click OK. Now the problem should be resolved.
View full article
S32 Design Studio (S32DS) for ARM supports IAR Plugin, and the user can use IAR specific features in S32DS with IAR toolchain for ARM. This document describes the way to convert S32DS project to IAR EW based project using project exporting wizard in S32DS. This guidance is based on the NXP S32K144 microcontroller, and compatible with S32K14x / S32K11x family.   The version of each IDE which is used for this document is as follows: S32 Design Studio for Arm 2018.R1 IAR Embedded Workbench for ARM 8.32.1.18631     1. Install IAR Plugin using IAR Embedded Workbench plugin manager on S32DS Help - Install New Software   Put "IAR Embedded Workbench for Eclipse " as the repository for new installation of software.     Help - IAR Embedded Workbench Plugin Manager     Install IAR Plugin which is matched with your IAR version.         2. Create S32DS Project File - New - S32DS Application Project   The tool chain should be chosen as IAR Toolchain. Be noted that the IAR 7.x toolchain is different from the IAR 8.x.   The project is created as follows.     3. Export S32DS Application Project File - Export   Choose S32 Design Studio - Project Info Export Wizard   Now "ProjectInfo.xml" was created. "ProjectInfo.xml" should be used for creating a project in the IAR EW.   4. Create IAR EW Project The way to create IAR project as described below. The snapshots are based on IAR EW 8.32.1. Details may vary.   5. Connect the Project Use the menu - Project - Add Project Connection, and choose "Freescale Processor Expert".   Select the "ProjectInfo.xml" file which was created at step #3.    Now, the project which had been created in IAR was connected to the S32DS project.   The created IAR project should be modified if the user wants to use the project with S32DS SDK to build and debug under IAR EW environment as follows.   1. Modify the Linker configuration and remove ProjectInfo.xml Remove "ProjectInfo.xml"   Linker configuration from the project Options   Even though the user modified the linker configuration, a definition in IAR EW  for "device_registers.h" from SDK will cause build error when trying building the project.   This error will be eliminated by inserting Chip specific definition into IAR project. If you take a look into the "device_register.h", you can find the definition as follows.   2. Define symbols  Right mouse click on the Project name - Options   Write the symbols referred from "device_register.h". The symbols may vary (e.g., CPU_S32K146, CPU_S32K142, ...).   3. Build and Debugger configuration Options - Debugger   I used PE micro's OpenSDA on S32K144EVB for this document. After choosing debugger and clicking Download and Debug (Ctrl+D), you can see the P&E Configuration Manager as follows. Just choose appropriate configuration, and select the correct part number of S32K by clicking Select New Device.   Finally, you can download and debug the converted IAR EW project with S32DS SDK.
View full article
This document shows the step-by-step process to create a simple blinking LED application for the S32G family using the S32 RTD AUTOSAR drivers. This example used for the S32G-VNP-RDB2 EVB, connected via ethernet connection through S32 Debugger. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32G development package and the S32 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. Launch S32 Design Studio for S32 Platform Procedure New S32DS Project OR Provide a name for the project, for example 'Blinking_LED_RTD_With_AUTOSAR'. The name must be entered with no space characters. Expand Family S32G2, Select S3G274A_Rev2 Cortex-M7 Click Next Click '…' button next to SDKs Check box next to PlatformSDK_S32XX_2022_07_S32G274A_Rev2_M7_0. Click OK And also, uncheck the other cores Cortex_M7_1 ,  Cortex_M7_2. Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents. To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file. Select the overview tab and disable Pins tool. Make sure to overview tab windows shows settings shown as below.  Here, we are disabling pin tools and using MCAL driver from peripheral tools for using AUTOSAR drivers. Now from Overview menu, select peripheral tools and double click to open it. In the driver sections, “Siul2_Port_1 driver” is the non-AUTOSAR version driver and so it must be replaced. Right click on ‘Siul2_Port_1’ and remove it. Keep the osif_1 driver as it is. Click on the ‘+’ next to the MCAL box. Locate and then select the ‘MCU’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Dio’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Port’ component from the list and click OK. Now components tab should show like below : Now we required to configure the different MCAL drivers that we added. Starting with Dio configuration, open the Dio configuration. Now, open the ‘DioGeneral’ tab, and select checkmark as per shown below: Now, open the ”DioConfig” tab. In that, select  “+” sign adjacent to Dio Channel. Then edit Name to Digital_Output_LED and “Dio Channel Id”  to ‘6’ instead of ‘0’. From the schematic for S32G-VNP-RDB2 EVB, we can select signal line based on your choice for the LED color for the multicolor RGB LED. Now, checking for blue user LED from the schematic, channel 6 is connected to blue LED signal, so we use channel 6 signal line to the chip on the blue LED. Similarly, so you can select signal line based on LED color you select. Now Select Port tab for Port configuration. And open the Port Configuration tab, and from that open “PortConfigSet” tab. Change the PortPin Mscr to 6 , PortPin Direction to PORT_PIN_INOUT. After change it should be as below. At the bottom you will find the “UnTouchedPortPin ’’ . Click on “+’’ and add PortPins. Now add 4 port pins as per below configuration. Pins 0, 1, 4, and 5 should be setup. Now configure MCU component. Select Mcu component in MCAL, and then open the Mcu configuration. In Mcu configuration select “McuModesettingConf” from the dropdown menu as shown below. Select ‘McuPartition0Config’ and deselect checkbox for CM7_0 Under MCU Control, CM7_1 Under MCU Control, CM7_2 Under MCU Control as marked below. And it should show as below Now select the Mcupartition1Config and uncheck checkmarks from the selection boxes as shown below Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar. To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective. If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added. Before anything else is done, Initialize the clock tree and apply PLL as system clock, Apply a mode configuration, Initialize all pins using the Port driver by adding – editing code before write code here comment in main function.          Mcu_Init(&Mcu_Config_BOARD_InitPeripherals);     /* Initialize the clock tree and apply PLL as system clock */     Mcu_InitClock(McuClockSettingConfig_0);     /* Apply a mode configuration */     Mcu_SetMode(McuModeSettingConf_0);     /* Initialize all pins using the Port driver */     Port_Init(NULL_PTR); Now replace the logic of for loop as shown below code section, which will enable the LED blinking for 10 times: First define the variable volatile uint8 level; globally above the main function. You also need to declare and initialize the loop variable uint8 i = 0U. Then replace the code as below: while (i++ < 10) {       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_HIGH);       level = Dio_ReadChannel(DioConf_DioChannel_Digital_Output_LED);       TestDelay(2000000);       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_LOW);       level = Dio_ReadChannel(DioConf_DioChannel_Digital_Output_LED);       TestDelay(2000000); } Before the 'main' function, add a delay function as follows: void TestDelay(uint32 delay); void TestDelay(uint32 delay) {     static volatile uint32 DelayTimer = 0;     while(DelayTimer<delay)     {         DelayTimer++;     }     DelayTimer=0; } Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application: Add #include "Mcu.h" #include "Port.h" #include "Dio.h" Build 'Blinking_LED_RTD_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'. After the build completes, check that there are no errors. Open Debug Configurations and select 'Blinking_LED_RTD_with_AUTOSAR_Debug_RAM'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist. And make selection as shown in screenshot below. You need to select the ethernet connection for S32 debugger and provide its IP address Click Debug To see the LED blink, click ‘Resume' This code as it is will blink the LED 10 times, you can make changes in for loop condition to blink it infinitely.
View full article
The Port_Ci_Port_Ip_Example in S32K1 RTD 1.0.1 lacks GPIO interrupt function. Port_Ci is part of Icu(Input Capture Unit), the main function of the example should have been: use the Icu and Dio drivers to toggle a LED on a push button. But it doesn't. So this document will show the step-by-step process to add 'GPIO interrupt' function in Port_Ci_Port_Ip_Example using the S32K1xx RTD and the S32 Configuration Tools. This example is for the S32K144EVB-Q100 EVB, connected to a PC through USB (OpenSDA) connection. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32K1xx development package and the S32K1 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools.   Launch S32 Design Studio for S32 Platform   Procedure 1. Import Port_Ci_Port_Ip_Example_S32K144 example File->New->S32DS Project from Example Although the main function mentions the example use the Icu and Dio drivers to toggle a LED on a push button, it actually just waits in a loop for a delay to blink the LED. Not sure why the implementation of GPIO interrupts(Port_Ci_Icu) is missing.   2. Add push button and LED in Pins tool Add the pins for user buttons (SW2 PTC12 and SW3 PTC13) and LEDRGB_RED (RGB_RED PTD15) according to the S32K144EVB schematic RB1.   3. Add IntCtrl_Ip component Go to Peripherals tool. Here we can see that the ‘Gpio_Dio’ and ‘Port’ components are already added. From the Components view, click on ‘Add a new configuration component…’ button from the Drivers category. This will bring up a list of non-AUTOSAR components. Locate and then select the ‘IntCtrl_Ip’ component from the list and click OK. Keep the default setting after add ‘IntCtrl_Ip’ component, we will call IntCtrl_Ip_InstallHandler and IntCtrl_Ip_EnableIrq those two APIs to install and enable the PORTC IRQ separately. (Here we didn't change the settings of ‘IntCtrl_Ip’, nor use IntCtrl_Ip_Init and IntCtrl_Ip_ConfigIrqRouting API to enable interrupts and install handlers in IntCtrl_Ip.)   4. Add Port_Ci_Icu component Locate and then select the ‘Port_Ci_Icu’ component from the list and click OK. Follow the steps below to configure it. Selecting PORT_2 for ICU Peripheral ISR Name and select IcuIsrEnable at step 6 actually refers to PORT C used in this example. In order to use the GPIO interrupts of the onboard SW2 (PTC12) and SW3 (PTC13) buttons, you need to add one more channel in step 9, and select Port CI Hardware Module and Hardware channel in steps 8 and 10. The button circuit has a pull-down resistor, and it will be pulled high after being pressed, so the rising edge trigger is selected. In step 14, add IcuSignalNotification for PTC12 and PTC13 respectively, that is, the notification after the corresponding GPIO pin input captures the rising edge (there is no need to clear the interrupt flag here, the RTD driver has already done it).   5. Include the headers for the drivers used in the application   6. Add Port_Ci_Icu drivers Port_Ci_Icu_Ip_Init initialize the rising edge of PTC12 and PTC13 set by the S32 Configuration Tools. Port_Ci_Icu_Ip_EnableNotification enable the Callback of PTC12 and PTC13 respectively, and we toggle the blue and red LEDs in the corresponding Callback.   7. Add IntCtrl drivers IntCtrl_Ip_InstallHandler installs the PORT_CI_ICU_IP_C_EXT_IRQ_ISR interrupt handler generated by the S32 Configuration Tools.
View full article
A vulnerability in the Apache Log4j was identified in the articles posted: CVE-2021-44228 and CVE-2021-45046 NXP has performed an analysis of this vulnerability with regard to the S32 Design Studio. Our conclusion is that the S32 Design Studio (all versions) is NOT IMPACTED. Although the Log4j is used by S32 Design Studio, the version used is 1.x and the vulnerability was introduced in version 2.12 with a combination of Java versions 9/10/11 where LDAP policy is enabled by default (CVE-2021-45046). The S32Design Studio installation environment is independent and based on Java 8 version, which is common for all tools running under S32Design Studio IDE. In addition, the S32 Design Studio does not use JMSAppender, so it is not affected by the identified log4j 1.x usage concern (CVE-2021-44228). When we determine an upgrade of the Log4j and/or Java version is required for a future release of S32 Design Studio, then this vulnerability will be addressed. Please see the attached presentation for details on other tools owned by NXP Automotive Processing Software Tools.
View full article
A typical debug session will begin by downloading code to Flash and then debugging from main() onwards. However, to explore an already running system a debug connection (attach) can be made to the target MCU without affecting the code execution (at least until the user chooses to halt the MCU!).   Note: Source level debug of a running target is only possible if the sources of the project to be attached exactly match the binary code running on the target.   Click the (Debug As) button on the toolbar, then click Debug Configurations from the drop-down menu. In the left pane of the Debug Configurations dialog box, expand the debugging interface specified in the project settings and click the required launch configuration. After you click the configuration in the left pane, the configuration settings appear in the right pane grouped in tabs. PEmicro Select the Startup tab, then set the ‘Attach to Running Target’ check box as below: When a debug connection is made, the target will continue running until it is paused.   SEGGER J-Link Select the Debugger tab, then set the ‘Connect to running target’ check box as below: Unfortunately, this feature currently not supported.
View full article
Watchpoints are Breakpoints for Data and are often referred to as Data Breakpoints. Watchpoints are a powerful aid to debugging and work by allowing the monitoring of global variables, peripheral accesses, stack depth etc. The number of watchpoints that can be set varies with the MCU family and implementation. Watchpoints are implemented using watchpoints units which are data comparators within the debug architecture of an MCU/CPU and sit close to the processor core. When configured they will monitor the processor’s address lines and other signals for the specific event of interest. This hardware is able to monitor data accesses performed by the CPU and force it to halt when a particular data event has occurred. The method for setting Watchpoints is rather more hidden within the IDE than some other debugging features. One of the easiest ways to set a Watchpoint is to use the Outline View. From this view you can locate global and static variables then simply select Toggle Watchpoints.     Once set, they will appear within the Breakpoints pane alongside any breakpoints that have been set.    Watchpoints can be configured to halt the CPU on a Read (or Load), Write (or Store), or both. Since watchpoints ‘watch’ accesses to memory, they are suitable for tracking accesses to global or static variables, and any data accesses to memory including those to memory mapped peripherals.  Note : To easily distinguish between Breakpoints and Watchpoints within the Breakpoint view, you can choose to group entries by Breakpoint type. From within the Breakpoints view, click the Eclipse Down Arrow Icon Menu, then you can select to Group By Breakpoint Types as shown below:   As you can see from the above graphic, the option to set a Watchpoint is also available directly from the Breakpoint view.   When set from here, you will be offered an unpopulated dialogue – simply entering an address will cause a watchpoint to be created, monitoring accesses to that location.     Another place to set Watchpoints within the IDE is from the context sensitive menu within a Memory view.   Unfortunately, the conditional watchpoints in S32 Design Studio for S32 Platform 3.3 may not work in some cases.
View full article
Condition: Enable Stopindebug bit for PIT and STM module. Counter could be stop when debug project, but when i set debug mode on, counter not count, project can't be run. Analysis: In order for PIT timer to count when a FRZ bit is enabled, all cores on S32V23x devices need to be running. The reason why it does not work out of the box with current plugin configuration, is because we halt all device cores, which is especially necessary for RAM based projects. Solution: We created a start-up macro to keep all cores running when S32V232M80 or S32V234M100 debug sessions are launched. In order to use it, please go to the following directory without your S32DS3.2 IDE: eclipse\plugins\com.pemicro.debug.gdbjtag.pne_4.2.8.201909091700\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx. Please rename S32V234M100_All_Cores_Running.mac or S32V232M80_All_Cores_Running.mac to default macro names, saving existing default macros in renamed form, or a separate location: S32V234M100.mac or S32V232M80.mac.separate location: S32V234M100.mac or S32V232M80.mac.
View full article
In this document, we show the steps to use the New Project Wizard to create a new application project for APEX2, ISP, or both.   1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 APEX2/ISP Linux' processor option 5. Click Next 6. Select the APEX2/ISP options you need.       a. APEX2 programming - will add support to your project for an APEX2 application, you need this for any new APEX2 project       b. APEX2 visual modeling - will create a separate project for your APEX2 program diagram, you need this to connect your APEX2 graph diagrams together. But you could also create it separately later. The APEX graph diagram must be created separately with another New Project Wizard.       c. ISP programming - will add support to your project for an ISP application, you need this for any new ISP project       d. ISP visual modeling - will create a separate project for your ISP data flow diagram, you will not need this if you plan to use an existing graph diagram. This can also be created later.       e. ISP static sequencer - by default, a dynamic sequencer is generated from your graph diagram, enable this to generate a static sequencer instead. This can be set/changed later in the Emit Configurations. 7. Click Finish 8. You now have a project or set of projects for development on the S32V234.
View full article
The following article describes how to add FreeRTOS thread aware debugging to the Eclipse Debug view using SEGGER J-Link: Show FreeRTOS Threads in Eclipse Debug View with SEGGER J-Link and NXP S32 Design Studio | MCU on Eclipse  I hope this is useful, Erich
View full article
Bare-metal project migration from an older version of S32DS into a newer one is typically pretty straightforward. Despite of that the migration into S32DS Power v1.2+ requires more attention due the fact it includes a new version of GCC compiler + GCC binutils (see the GCC release notes - here). This version of GCC is now fully EABI VLE compliant  (in contrast to previous versions of S32DS Power  v1.0 and v1.1) and it has several consequences for the project migration object code/libraries are not backward compatible - if you have an object code/library built by a previous version of S32DS Power v1.x you have to rebuild it in new S32DS v1.2+ compiler. default compiler setup has changed - bitfield access is not volatile anymore. This may have a impact on a peripheral registers access via standard header file bitfield structures. Such access may require a specific load/store instruction e.g. "stw" but if compiler is allowed to optimize the access (e.g. use "stb" instead of "stw") an exception may occur. Therefore it is recommended to add  -fstrict-volatile-bitfields  flag into your project GCC compiler settings: linker script file (*.ld) requires some additional linker sections - Linker script file in S32DS Power v1.2+ must contain the sections below: •  KEEP for .init and .fini sections • .ctors and .dtors sections • .preinit array .init array and .fini array sections If the linker script file is not updated and the linker warnings are ignored you may experience an exception at the runtime - typically when __init routine is executed. Missing .init section causes that an invalid instructions is fetched and causes the core IVOR exception. There is an easy way how to automatically fix the linker script file issue directly in IDE. If you import and build an older project in S32DS Power v1.2 the linker issues these linker script related warnings: Right click on the warning and select Quick Fix: Select "Add missed section in linker script"  + "Select All" and press "Finish". Repeat these steps until all the linker script warnings disappears. If you don't use IDE project you have to add the sections below into your linker script manually: .text_vle : { INPUT_SECTION_FLAGS (SHF_PPC_VLE) *(.text.startup) *(.text) *(.text.*) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(16); } > m_text /* that will force pick VLE .text sections */ .ctors : { __CTOR_LIST__ = .; /* gcc uses crtbegin.o to find the start of the constructors, so we make sure it is first. Because this is a wildcard, it doesn't matter if the user does not actually link against crtbegin.o; the linker won't look for a file to match a wildcard. The wildcard also means that it doesn't matter which directory crtbegin.o is in. */ KEEP (*crtbegin.o(.ctors)) KEEP (*crtbegin?.o(.ctors)) /* We don't want to include the .ctor section from from the crtend.o file until after the sorted ctors. The .ctor section from the crtend file contains the end of ctors marker and it must be last */ KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)) KEEP (*(SORT(.ctors.*))) KEEP (*(.ctors)) __CTOR_END__ = .; } > m_text .dtors : { __DTOR_LIST__ = .; KEEP (*crtbegin.o(.dtors)) KEEP (*crtbegin?.o(.dtors)) KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)) KEEP (*(SORT(.dtors.*))) KEEP (*(.dtors)) __DTOR_END__ = .; } > m_text .preinit_array : { PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } > m_text .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } > m_text .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } > m_text‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ This may help you to avoid time consuming debugging to figure out the root cause of the core exception. 
View full article
Perhaps you are just using the S32DS for Power for the first time, and maybe you've seen the provided examples and want to learn a bit more about how they were created. Here are the steps to create a simple application for the MCP5748G MCU which toggles a pin causing one of the user LEDs to blink. This example includes use of the S32 SDK for Power Architecture. Please note: There are options in the steps below to cover the case of either the DEV-KIT(DEVKIT-MPC5748G) or Motherboard(X-MPC574XG-MB) with Daughtercard(X-MPC574XG-324DS) hardware EVBs. 1) Launch S32DS for Power 2) Select File -> New -> New S32DS Project 3) Enter a name for the project, such as 'BlinkingLED' 4) Locate, from the list of processors, Family MPC574xG -> MPC5748G, and select it. 5) Click Next 6) Uncheck the boxes for cores e200z4 and e200z2, leaving just e200z4 (boot) checked. This is because the application will run on the boot core and will not use either of the other two cores. 7) Click on the '…' button next to SDKs, in the column for BlinkingLED_Z4_0. 😎 Check the box next to MPC5748G_SDK_Z4_0_GCC to include support for the SDK within the new project and for the core we have selected. 9) Click OK 10) Click Finish to close the New Project wizard window and start the project generation. 11) Wait a minute or two for the project generation script to complete. 12) Go to the 'Components Library' view then locate and double-click on 'pit' component to add it to the project.  Alternatively, right-click and select Add to project. You can verify it was added by inspecting the 'Components - <project_name>' view. 13) With 'pit' selected in the 'Components - BlinkingLED_Z4_0' view, go to the 'Component Inspector' view to see the configurations for the PIT component. Locate the section for 'Configuration 0'. You may have to scroll down to see it. Change the 'Time period' setting to 500000 microsec(0.5 sec). Note that we are editing the settings for Clock configuration 'clockMan_InitConfig0', you will need the name of this configuration later. 14) Back in the 'Components' view, select 'pin_mux' component and return to the 'Component Inspector' view 15) From the 'Routing' tab, select the 'SIUL2' sub-tab and scroll down the Signals list until 'GPIO_0' (DEV-KIT) or 'GPIO_99' (Motherboard) is shown. 16) Change to the following settings: a. Pin/Signal Selection: PA[0] (DEV-KIT) / PG[3] (Motherboard) b. Direction: Output Pin PA0/PG3 is connected to user LED 2 on the evaluation board. 17) All configuration settings are now complete. Click Generate Processor Expert code button in the 'Components' view or use the menu bar Project-> Generate Processor Expert Code. 18) Wait for the code generation to complete. 19) Now, from the 'Project Explorer' view, the generated code is visible in the folder 'Generated_Code' of the project 'BlinkingLED_Z4_0'. 20) If not already open, in 'Project Explorer' open the file 'BlinkngLED_Z4_0\Sources\main.c' by double-click. This will open the file in the editor view. 21) Scroll down until the following comments are shown: /* Write your code here */ /* For example: for(;;) { } */ We need to add some code here to initialize the clocks, timers and pins. Then we will setup a timer interrupt handler to toggle the pin. 22) First we need to initialize the clocks. From the 'Components' view, expand 'clock_manager' and then drag & drop CLOCK_DRV_Init function into main() of main.c, just after the comments identified in the previous step within the text editor view. 23) Add to the function CLOCK_DRV_Init(), the parameter &clockMan1_InitConfig0 to give it the address of the user configuration structure generated by ProcessorExpert in '.../Generated_Code/clockMan1.c'. This is the clock configuration for which we edited the timer period in an earlier step. 24) Next we need to initialize the pins. Back in the 'Components' view, expand the 'pin_mux' then drag and drop the function PINS_DRV_Init after the clock initialization. 25) Again from the 'Components' view, expand 'interrupt_manager', then drag & drop INT_SYS_InstallHandler in 'main()'. This installs the PIT channel 0 interrupt handler. 26) Enter the parameters: PIT_Ch0_IRQn, &pitCh0Handler, NULL 27) In the User includes section at the start of main.c, add the implementation of the handler a. Create a function called pitCh0Handler b. In the function body: clear the interrupt flag and toggle LED   /* IRQ handler for PIT ch0 interrupt */   void pitCh0Handler(void)   { /* Clear PIT channel 0 interrupt flag */ PIT_DRV_ClearStatusFlags(INST_PIT1, 0U); /* Toggle LED (GPIO 0 connected to user LED 2) */ SIUL2->GPDO[0] ^= SIUL2_GPDO_PDO_4n_MASK; // DEV-KIT /* SIUL2->GPDO[99/4] ^=SIUL2_GPDO_PDO_4n3_MASK;*/ // Motherboard   } Note: Get PIT_DRV_ClearStatusFlags by drag & drop from the 'pit' component. 28) In 'Components' view, expand 'pit' component and then drag & drop PIT_DRV_Init, PIT_DRV_InitChannel & PID_DRV_StartChannel in main() after INT_SYS_InstallHandler(). 29) Fill in the second parameter of the last function(channel number): 0U 30) Build the code. Click the down arrow next to the 'Build' button and select Debug_RAM. Check that there are no build errors. 31) Enter the 'Debug Configurations' menu: a. From the menu bar, Run -> Debug Configurations... b. From the toolbar, down arrow next to Debug button -> Debug Configurations... 32) The Debug Configurations window appears. Select the configuration BlinkingLED_Z4_0_Debug_RAM from within the GDB PEMicro Interface Debugging group. 33) Select the 'Debugger' tab to setup the connection to the debugger hardware device. 34) Select the PEMicro Interface which corresponds to your setup: a. If using the motherboard, you will likely use the USB Multilink, which is connected to your PC via USB cable (type A on one end, type B on the other) and is connected to the motherboard via the 14-pin JTAG cable. b. If using the DEV-KIT board, you will likely choose the OpenSDA, which is integrated into the DEV-KIT board and is connected with just a USB cable (type A on one end, type micro on the other). 35) Click Debug To launch the debugging session. This will also open the Debug perspective. 36) In the Debug perspective, once the debugging session has fully launched, the code will be executed to the start of main(), where a breakpoint was automatically set for you. Press Resume button in the toolbar, Run -> Resume in the menu bar, or F8 on your keyboard to run the application. 37) You should now see the User LED2 on the board blink every 0.5 seconds. 38) To see the value of the output register bit for the output pin connected to the LED: a. Set a breakpoint on a line within pitCh0Handler() b. Go to the EmbSys Registers view, expand the SIUL2 module and scroll down to the GPDO register index which is accessed in the code. Double-click it to read the value. Expand it to see the individual bits. c. Press Resume a few times to see the register value change
View full article
This document describes two ways how to add a static library file (*.a) into your S32 Design Studio GCC project. These methods differs from each other in sense how a library update is reflected into project build process. Adding a static library WITHOUT dependency to executable (elf) file This approach assumes a library does not change. An update of the library does not trigger project rebuild process. If the library changes the project needs to be manually cleaned (assuming no other source file has changed) and next build links the updated library. The path to the library and the library name shall be entered into Project Properties -> C/C++ Build -> Settings -> Standard S32DS C Linker -> Libraries Please note that GCC adds prefix "lib" and the extension ".a"  to the library name entered into the above dialog by default. GCC linker will search for the library file named: "libtestlib.a" in the folder "c:\my_libs" In the example above. In case a library cannot be found the linker error occurs e.g. one depicted below. The linker library file name option "-ltestlib.a" is expanded into file name "libtestlib.a.a" which does not exist. 10:28:53 **** Incremental Build of configuration Debug for project S32K144_Project_with_library **** make -j8 all Building target: S32K144_Project_with_library.elf Executing target #5 S32K144_Project_with_library.elf Invoking: Standard S32DS C Linker arm-none-eabi-gcc -o "S32K144_Project_with_library.elf" "@S32K144_Project_with_library.args" c:/nxp/s32ds_arm_v2.0/cross_tools/gcc-arm-none-eabi-4_9/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -ltestlib.a collect2.exe: error: ld returned 1 exit status make: *** [makefile:49: S32K144_Project_with_library.elf] Error 1 10:28:54 Build Finished (took 1s.332ms)‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ For a custom library name add colon character ":" at the beginning of the library name to disable the default prefix/extension expansion. GCC linker now searches for file name "testlib.lib" in the example below:   Adding a static library WITH dependency to executable (elf) file If a static library has changed - "touched"  it is sometimes desired to trigger project rebuild. In this scenario the library shall be added into a different project dialog: Project Properties -> C/C++ Build -> Settings -> Standard S32DS C Linker -> Miscellaneous -> Other objects The items from "Other objects" list is propagated into USER_OBJS makefile variable which is prerequisite for auto-generated makefile rule that build the target (elf): Enjoy linking static libraries in S32DS!
View full article
Sometimes you would like to share sources between projects and - even better - between platforms. Let's say that we are developing software with the very same functionality for S32K144 and MPC5744P. In this case, we can identify platform independent functions - generic, platform specific functions - not related to MCU itself, but related to the way some peripheral works (for example different ADC result range) - and MCU dependent functions like clock init. In attachment is a very simple SDK which can be shared with S32K144 and MPC5744P (each in different S32DS editions).  Unzip my_sdk.zip archive (for example C:\NXP folder). You can import example projects, but instead let's start from the beginning. Create a new S32DS Application project and choose MCU: You can use default project configurations and click through to finish: Right click on project name -> Properties and select SDKs -> Add Complete the Name, Version and Description fields in New SDK dialog and click on Change button next to Location field. In Change SDK Location dialog, leave Define new variable setting selected, click Browse and find the my_sdk path: Now we can select files (sources, headers...) from selected SDK, you can select all available files. If you select a folder, then all files in that folder will be selected as well. Don't forget to select header files too: If you choose Copy - the files will be copied into project folder and you can do local changes. Without this option (default) - changes will be shared between all projects depended on this particular SDK. The ability to individually select the files to be included from the SDK as well as to copy into the project folder, provides much flexibility to customize SDK usage in your projects. Click on OK, then Attach/Detach... to attach this SDK into your project:  If you like to use your SDK for newly created projects (as an option in SDK select list) - click on Make global button: Now you can see changes in your project: As well, the SDK can be viewed in SDK Explorer (Window -> Show View -> Other...), where functions and macros are available for drag and drop functionality into your code: Platform specific code is filtered by preprocessor-defined macro. So - let's define if we are working with S32K144 or MPC5744P. Right click on project name -> Properties -> C/C++ Build -> Settings -> <Standard S32DS C Compiler OR name of your compiler> -> Preprocessor: We are done - now we can use SDK functions - S32K144:  and MPC5744P (enabling interrupts is default part of empty project for MPC5744P - that's only difference):
View full article
In this document, we show the steps to use the New Project Wizard to create a new application project for APEX2, ISP, or both.   1. Launch S32DS for Vision 2. Select File -> New -> S32DS Application Project 3. Enter a name for the project 4. Select the 'A53 APEX2/ISP Linux' processor option 5. Click Next 6. Select the APEX2/ISP options you need.       a. APEX2 programming - will add support to your project for an APEX2 application, you need this for any new APEX2 project       b. ISP programming - will add support to your project for an ISP application, you need this for any new ISP project       c. ISP visual modeling - will create a separate project for your ISP data flow diagram, you will not need this if you plan to use an existing graph diagram. This can also be created later. 7. Select the SDK(s) as appropriate for your setup. For example, 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS, the one which corresponds to your OS is selected for you by default. 7. Click Finish 8. You now have a project or set of projects for development on the S32V234.
View full article
PEmicro’s GDB Server can take advantage of four useful SWO debug tools: Power Measurement SWO ITM Console SWO Data capture Real-Time Expressions. This document describes how to enable and use these features. Note: To set up streaming for SWO debug features, the user should check the “Enable Streaming” checkbox in Debug Configurations during setup. Then the port should be specified in the Streaming Server Port text box. Hardware Requirements The following versions (or later) of PEmicro hardware interfaces are required to take advantage of SWO streaming functionality: Multilink FX Rev. C Multilink Universal Rev. D Multilink ACMP Rev. B Real-Time Power Measurement To enable Power Measurement capture, an active debug session must already be in process. Click the Gear Icon on the title bar of the PEmicro "Power Measurement” window. Select the frequency of data capture and check the Enable box. After clicking OK, Power Recording is now active. Note:    The Multilink FX debug probe is required for Real-Time Power Measurement Power Configuration Dialog The next time the target MCU is run, real-time power measurement readings will be shown. The user can start/stop power recording, zoom, export data, and more SWO Printf Console The SWO Printf Console will display messages which are streamed through the SWO pin and captured by the Multilink. There are two main configuration steps needed to leverage this feature. First, the project must be configured to re-direct the printf() statements to the SWO Printf peripheral. This is done at project creation time. Second, the green "Play" button on the SWO ITM Console needs to be clicked during an active debug session. This will cause data collection of SWO printf information to occur on the next Resume. Once data is streaming, the red “Stop” button will stop data streaming. Printf() Statements Displayed In SWO ITM Console The Multilink automatically measures the data communication rate on the SWO pin and adjusts to it automatically. This auto-detect sequence is done each time the processor is stopped in debug mode. If the running code changes the core frequency, a breakpoint should be set after the frequency change so the Multilink can adjust to the new SWO communications rate (which is a function of the core frequency). SWO Data capture The SWO Data view allows the user to configure variables to be tracked such that any reads and writes to these variables are captured and streamed to the Multilink via the SWO pin. This view shows all of the realtime access which have occurred along with the timing of the different accesses. For SWO data, there is a bit more setup.  The user needs to select the 'Eyeglasses+' symbol which will bring up a popup of Add datawatch items.  Simply enter the information of the different variables to be tracked. Up to four separate variables can be tracked simultaneously. In this example, we select that we wish to capture read and writes of the ledsOn and seconds variables. Once added, the user needs to select which watches data will be captured by checking the "Enable trace" boxes in the SWO Data window and then click the Green Arrow to set the program to start capture on Resume.Upon resuming the application, the right side of the window will show the access which are occurring. Note that this happens in real-time; the microcontroller is not stopped when accesses occur (i.e. the is separate from data breakpoints). Variable Read/Writes Displayed In Real Time The Multilink automatically measures the data communication rate on the SWO pin and adjusts to it automatically. This auto-detect sequence is done each time the processor is stopped in debug mode. If the running code changes the core frequency, a breakpoint should be set after the frequency change so the Multilink can adjust to the new SWO communications rate (which is a function of the core frequency). Real-Time Expressions This view is similar to the standard Eclipse "Expressions" window with the exception that its contents will update in real-time without the device being halted in debug mode. Just add the appropriate variables to the Real Time Expressions window and you will see them updating in real-time. Add Variables To Real-Time Expressions Windows
View full article