Sleep Mode for S12ZVL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sleep Mode for S12ZVL

2,576 Views
DELPHI_Eric
Contributor III

Sleep function: When an event occurs when the time, 25 ± 0.1 seconds, the system shut down all the load, the system into the sleep mode;Sleep Mode for S12ZVL.

Can S12ZVL achieve this function?

Can S12 resume sleep before S12 wake up from sleep mode?

If I choose the Pseudo Stop Mode,is this mode?

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,808 Views
iggi
NXP Employee
NXP Employee

Hi Shen,

i am sorry but i don;t understand what you are saying here.

In Pseudo Stop mode - In this mode the system clocks are stopped but the oscillator is still running and
the real time interrupt (RTI), watchdog (COP) and Autonomous Periodic Interrupt (API) may
be enabled. Other peripherals are turned off. This mode consumes more current than system
STOP mode but, as the oscillator continues to run, the full speed wake up time from this mode
is significantly shorter.

Here are some SW example demonstrating Stop mode functionality:

SW examples for MagniV S12ZVC and S12ZVL devices 

or this one (you can re-use main.c for S12ZVL)

Low power mode example code for MagniV S12ZVC device 


Have a great day,
iggi

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------