Low power mode example code for MagniV S12ZVC device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Low power mode example code for MagniV S12ZVC device

No ratings

Low power mode example code for MagniV S12ZVC device

The example code demonstrates MCU low power modes: STOP and WAIT. For detailed description see main.c file of the project.

* - tested on X-VLG-S12ZVC board

* - BUSCLK = 6.25MHz based on internal oscillator clock IRCCLK = 1MHz.The PLL set by default in PEI mode.

* - Reference documentation:

MC9S12ZVCRMV1.pdf (REV 1.9)

VLG-MC9S12ZVC-SCH.pdf (Document Number SCH-28038, SPF-28038)

Labels (1)
Attachments
Comments

Hi guys,
It seems that the link is broken "Error 404 file not found".

Hi Alexis,

It has been updated.

Thanks.

Regards,

Daniel

Hi Daniel, 
Thank you very much for the effort.

Best regards,
Alexis

Hi guys,

where I can find the file EX-TIC-S12ZVC-STOPandWAITmode-CW106.zip?

The link seems to be broken "Not Found The item does not exist. It may have been deleted".

Regards

Hi Paolo,

It has been fixed, thank you,

BR, Daniel

Version history
Last update:
‎08-19-2015 07:30 AM
Updated by: