usb bdm multilink适用于s12zvm系列cpu吗?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb bdm multilink适用于s12zvm系列cpu吗?

636 Views
wangxin1
Contributor I

请问PART#USB-ML-12E这款调试器适用于9s12zvm系列cpu吗?谢谢!

Labels (1)
0 Kudos
Reply
2 Replies

463 Views
RadekS
NXP Employee
NXP Employee

Hi,

According to my information, the USB BDM Multilink (USB-ML-12E (Rev C.)) isn’t supported by P&E driver under Win10 as the legacy product. The debugger works correctly at our Win7 PCs.

So, if you have PC with Win10, you will probably need some newer debugger.

Optionally you may contact P&E support at www.pemicro.com

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

463 Views
iggi
NXP Employee
NXP Employee

Hi,

I understood the question somehow using online translator...

Yes, you can use USB-ML-12E (Rev C.) device to debug/program MagniV device based on S12Z core. We are using it on daily.

Have a great day,
iggi

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply