S12ZVC interrupt priority

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S12ZVC interrupt priority

跳至解决方案
5,408 次查看
xiaohui200808
Contributor III

Hello

      I see the S12ZVC datasheet:two registers  INT_CFADDR and INT_CFDATA0-7.There is something I donot understand.

Is it means S12ZVC can deal at most 8 interrupts at a point. By configure the  INT_CFDATA0-7 ,am I able to deal an interrupt at first ,whose interrupt priority is lower. when two interrupts occuered. IS there any demo code to describe it .Thank you!

标签 (1)
0 项奖励
回复
1 解答
4,802 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

For example, S12ZVML12_Hall_BLDC demo uses the below function:

/*****************************************************************************
*
* Function: void InitINT(void)
*
* Description: Interrupt priorities configuration
*
*****************************************************************************/
void InitINT(void)
{
 // set ADC 0 done ISR (0x184) priority to 6
 // 0x184 / 4 = 0x61 => reg. 0x60, offset 1
 INT_CFADDR = 0x60;
 INT_CFDATA1 = 6;
 
 // set ADC 0 error ISR (0x18C) priority to 2
 // 0x18C / 4 = 0x63 => reg. 0x60, offset 3
 INT_CFADDR = 0x60;
 INT_CFDATA3 = 2;
 
 // TIM ch1 input capture ISR (0x1C8) priority set to 5
 // 0x1C8 / 4 = 0x72 => reg. value = 0x70 + offset 2
 INT_CFADDR = 0x70;
 INT_CFDATA2 = 5;
 
 // TIM ch3 output compare ISR (0x1C0) priority set to 4
 // 0x1C0 / 4 = 0x70 => reg. value = 0x70 + offset 0
 INT_CFADDR = 0x70;
 INT_CFDATA0 = 4;
}

Regards,

Daniel

在原帖中查看解决方案

0 项奖励
回复
5 回复数
4,802 次查看
martynek
Contributor II

Hi,

There is the paging mechanism. You can configure all 128 interrupts priority with only 9 registers.

For instance, if you want to have two interrupts with different priority, let’s say:

CAN receive (Vector base + 0x154) and Port L (Vector base + 0x0C0)

 

Then for CAN receive interrupt:

Vector address/vector size = 0x154 / 4 = 0x55. We use only bit [7..4] for INT_CFADDR configuration. In this case, it is 0x50.

INT_CFADDR = 0x50;

 

The 3 LSB of 0x55 are 0b101 = 5, therefore for priority configuration of this interrupt use data register 5 and load it with priority you need.

INT_CFDATA5_PRIOLVL = 0x01;                   /*Priority level of CAN receive */

 

Similarly for Port L

INT_CFADDR = 0x30;

INT_CFDATA0_PRIOLVL = 0x02;                   /* Priority level of Port L */

The higher PRIOLVL number means the higher interrupt priority. With PRIOLVL = 0 the corresponding interrupt is disabled.

If more than one interrupt request is configured to the same interrupt priority level the interrupt request with the higher vector address wins.

You may look at S12Z CPU RM for more details about interrupt event principles:

http://www.nxp.com/assets/documents/data/en/reference-manuals/S12ZCPU_RM_V1.pdf

I hope it helps you.

Have a great day,

Daniel

4,802 次查看
simonliu
Contributor III

Hi Daniel,

     As mentioned above,If I need set the CAN and Port L priority at same time.How do I set INT_CFADDR?The CAN is 0x50,Port L is 0x30. I need set INT_CFADDR = (0x50 & 0x30 )?

0 项奖励
回复
4,802 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The INT_CFADDR registers selects 8 vectors out of 128 that are accessible in the 8-byte register window INT_CFDATA0–7. And thus you can't configure CAN and Port L interrupts with just one write to the INT_CFADDR register. You have to configure the interrupts one by one.

Regards,

Daniel

0 项奖励
回复
4,802 次查看
simonliu
Contributor III

Hi Daniel,

 

          I have set the reg for this,but it still doesn't work.

     pastedImage_1.png

          Is there an example of this part of the project?Tks!

0 项奖励
回复
4,803 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

For example, S12ZVML12_Hall_BLDC demo uses the below function:

/*****************************************************************************
*
* Function: void InitINT(void)
*
* Description: Interrupt priorities configuration
*
*****************************************************************************/
void InitINT(void)
{
 // set ADC 0 done ISR (0x184) priority to 6
 // 0x184 / 4 = 0x61 => reg. 0x60, offset 1
 INT_CFADDR = 0x60;
 INT_CFDATA1 = 6;
 
 // set ADC 0 error ISR (0x18C) priority to 2
 // 0x18C / 4 = 0x63 => reg. 0x60, offset 3
 INT_CFADDR = 0x60;
 INT_CFDATA3 = 2;
 
 // TIM ch1 input capture ISR (0x1C8) priority set to 5
 // 0x1C8 / 4 = 0x72 => reg. value = 0x70 + offset 2
 INT_CFADDR = 0x70;
 INT_CFDATA2 = 5;
 
 // TIM ch3 output compare ISR (0x1C0) priority set to 4
 // 0x1C0 / 4 = 0x70 => reg. value = 0x70 + offset 0
 INT_CFADDR = 0x70;
 INT_CFDATA0 = 4;
}

Regards,

Daniel

0 项奖励
回复