S12ZVC interrupt priority

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC interrupt priority

ソリューションへジャンプ
5,509件の閲覧回数
xiaohui200808
Contributor III

Hello

      I see the S12ZVC datasheet:two registers  INT_CFADDR and INT_CFDATA0-7.There is something I donot understand.

Is it means S12ZVC can deal at most 8 interrupts at a point. By configure the  INT_CFDATA0-7 ,am I able to deal an interrupt at first ,whose interrupt priority is lower. when two interrupts occuered. IS there any demo code to describe it .Thank you!

ラベル(1)
0 件の賞賛
返信
1 解決策
4,903件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

For example, S12ZVML12_Hall_BLDC demo uses the below function:

/*****************************************************************************
*
* Function: void InitINT(void)
*
* Description: Interrupt priorities configuration
*
*****************************************************************************/
void InitINT(void)
{
 // set ADC 0 done ISR (0x184) priority to 6
 // 0x184 / 4 = 0x61 => reg. 0x60, offset 1
 INT_CFADDR = 0x60;
 INT_CFDATA1 = 6;
 
 // set ADC 0 error ISR (0x18C) priority to 2
 // 0x18C / 4 = 0x63 => reg. 0x60, offset 3
 INT_CFADDR = 0x60;
 INT_CFDATA3 = 2;
 
 // TIM ch1 input capture ISR (0x1C8) priority set to 5
 // 0x1C8 / 4 = 0x72 => reg. value = 0x70 + offset 2
 INT_CFADDR = 0x70;
 INT_CFDATA2 = 5;
 
 // TIM ch3 output compare ISR (0x1C0) priority set to 4
 // 0x1C0 / 4 = 0x70 => reg. value = 0x70 + offset 0
 INT_CFADDR = 0x70;
 INT_CFDATA0 = 4;
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,903件の閲覧回数
martynek
Contributor II

Hi,

There is the paging mechanism. You can configure all 128 interrupts priority with only 9 registers.

For instance, if you want to have two interrupts with different priority, let’s say:

CAN receive (Vector base + 0x154) and Port L (Vector base + 0x0C0)

 

Then for CAN receive interrupt:

Vector address/vector size = 0x154 / 4 = 0x55. We use only bit [7..4] for INT_CFADDR configuration. In this case, it is 0x50.

INT_CFADDR = 0x50;

 

The 3 LSB of 0x55 are 0b101 = 5, therefore for priority configuration of this interrupt use data register 5 and load it with priority you need.

INT_CFDATA5_PRIOLVL = 0x01;                   /*Priority level of CAN receive */

 

Similarly for Port L

INT_CFADDR = 0x30;

INT_CFDATA0_PRIOLVL = 0x02;                   /* Priority level of Port L */

The higher PRIOLVL number means the higher interrupt priority. With PRIOLVL = 0 the corresponding interrupt is disabled.

If more than one interrupt request is configured to the same interrupt priority level the interrupt request with the higher vector address wins.

You may look at S12Z CPU RM for more details about interrupt event principles:

http://www.nxp.com/assets/documents/data/en/reference-manuals/S12ZCPU_RM_V1.pdf

I hope it helps you.

Have a great day,

Daniel

4,903件の閲覧回数
simonliu
Contributor III

Hi Daniel,

     As mentioned above,If I need set the CAN and Port L priority at same time.How do I set INT_CFADDR?The CAN is 0x50,Port L is 0x30. I need set INT_CFADDR = (0x50 & 0x30 )?

0 件の賞賛
返信
4,903件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The INT_CFADDR registers selects 8 vectors out of 128 that are accessible in the 8-byte register window INT_CFDATA0–7. And thus you can't configure CAN and Port L interrupts with just one write to the INT_CFADDR register. You have to configure the interrupts one by one.

Regards,

Daniel

0 件の賞賛
返信
4,903件の閲覧回数
simonliu
Contributor III

Hi Daniel,

 

          I have set the reg for this,but it still doesn't work.

     pastedImage_1.png

          Is there an example of this part of the project?Tks!

0 件の賞賛
返信
4,904件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

For example, S12ZVML12_Hall_BLDC demo uses the below function:

/*****************************************************************************
*
* Function: void InitINT(void)
*
* Description: Interrupt priorities configuration
*
*****************************************************************************/
void InitINT(void)
{
 // set ADC 0 done ISR (0x184) priority to 6
 // 0x184 / 4 = 0x61 => reg. 0x60, offset 1
 INT_CFADDR = 0x60;
 INT_CFDATA1 = 6;
 
 // set ADC 0 error ISR (0x18C) priority to 2
 // 0x18C / 4 = 0x63 => reg. 0x60, offset 3
 INT_CFADDR = 0x60;
 INT_CFDATA3 = 2;
 
 // TIM ch1 input capture ISR (0x1C8) priority set to 5
 // 0x1C8 / 4 = 0x72 => reg. value = 0x70 + offset 2
 INT_CFADDR = 0x70;
 INT_CFDATA2 = 5;
 
 // TIM ch3 output compare ISR (0x1C0) priority set to 4
 // 0x1C0 / 4 = 0x70 => reg. value = 0x70 + offset 0
 INT_CFADDR = 0x70;
 INT_CFDATA0 = 4;
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Regards,

Daniel

0 件の賞賛
返信