Regarding EEPROM 2 bit ECC Machine exception

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding EEPROM 2 bit ECC Machine exception

1,530件の閲覧回数
pratibhasurabhi
Contributor V

The EEPROM Flash 2 bit fault will generate a machine exception.

Will this case hold true if we "simulate" the double bit fault by setting the FDFD bit.

タグ(2)
0 件の賞賛
返信
1 返信

1,313件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Pratibha,

no, forcing the DFDF status bit by setting FDFD (see Section 20.3.2.5) has effect only on the DFDF status bit value and does not result in an invalid access.

SeeS12Z - Simulating ECC errors at EEPROM by cumulative write example code for more details regarding simulating machine exception due to double bit ECC error.


I hope it help you

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信