Regarding EEPROM 2 bit ECC Machine exception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding EEPROM 2 bit ECC Machine exception

1,487 Views
pratibhasurabhi
Contributor V

The EEPROM Flash 2 bit fault will generate a machine exception.

Will this case hold true if we "simulate" the double bit fault by setting the FDFD bit.

Tags (2)
0 Kudos
Reply
1 Reply

1,270 Views
RadekS
NXP Employee
NXP Employee

Hi Pratibha,

no, forcing the DFDF status bit by setting FDFD (see Section 20.3.2.5) has effect only on the DFDF status bit value and does not result in an invalid access.

SeeS12Z - Simulating ECC errors at EEPROM by cumulative write example code for more details regarding simulating machine exception due to double bit ECC error.


I hope it help you

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply