Regarding EEPROM 2 bit ECC Machine exception

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding EEPROM 2 bit ECC Machine exception

1,105 次查看
pratibhasurabhi
Contributor V

The EEPROM Flash 2 bit fault will generate a machine exception.

Will this case hold true if we "simulate" the double bit fault by setting the FDFD bit.

标记 (2)
0 项奖励
回复
1 回复

888 次查看
RadekS
NXP Employee
NXP Employee

Hi Pratibha,

no, forcing the DFDF status bit by setting FDFD (see Section 20.3.2.5) has effect only on the DFDF status bit value and does not result in an invalid access.

SeeS12Z - Simulating ECC errors at EEPROM by cumulative write example code for more details regarding simulating machine exception due to double bit ECC error.


I hope it help you

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复