Hello,
Let me just clarify.
There are specs about PP1,3 and 5 on S12ZVL RM rev1.01 Table A-9 #12&13
Maximum allowed continuous current Ipp : -10 — +25 mA
Over-current Detect Threshold IOCD : +40 — +80 mA
About these specs for sum of PP1,3 and 5? or for each port?
Best Regards,
Ikki
Solved! Go to Solution.
Hello Ikki
These specifications are valid for each individual pin.
However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.
Regards
DPB
Hello Ikki
These specifications are valid for each individual pin.
However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.
Regards
DPB
Hello DPB san,
Thank you! It makes sense to me!
Ikki