Ipp and IOCD on S12ZVL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ipp and IOCD on S12ZVL

ソリューションへジャンプ
2,273件の閲覧回数
ikkishingu
Contributor II

Hello,

 

Let me just clarify.

There are specs about PP1,3 and 5 on S12ZVL RM rev1.01 Table A-9 #12&13

  Maximum allowed continuous current Ipp : -10 — +25 mA

  Over-current Detect Threshold IOCD : +40 — +80 mA

About these specs for sum of PP1,3 and 5? or for each port?

 

Best Regards,

Ikki

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,145件の閲覧回数
DPB
NXP Employee
NXP Employee

Hello Ikki

These specifications are valid for each individual pin.

However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.

Regards

DPB

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,146件の閲覧回数
DPB
NXP Employee
NXP Employee

Hello Ikki

These specifications are valid for each individual pin.

However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.

Regards

DPB

0 件の賞賛
返信
2,145件の閲覧回数
ikkishingu
Contributor II

Hello DPB san,

Thank you! It makes sense to me!

Ikki

0 件の賞賛
返信