Ipp and IOCD on S12ZVL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ipp and IOCD on S12ZVL

Jump to solution
2,281 Views
ikkishingu
Contributor II

Hello,

 

Let me just clarify.

There are specs about PP1,3 and 5 on S12ZVL RM rev1.01 Table A-9 #12&13

  Maximum allowed continuous current Ipp : -10 — +25 mA

  Over-current Detect Threshold IOCD : +40 — +80 mA

About these specs for sum of PP1,3 and 5? or for each port?

 

Best Regards,

Ikki

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,153 Views
DPB
NXP Employee
NXP Employee

Hello Ikki

These specifications are valid for each individual pin.

However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.

Regards

DPB

View solution in original post

0 Kudos
Reply
2 Replies
2,154 Views
DPB
NXP Employee
NXP Employee

Hello Ikki

These specifications are valid for each individual pin.

However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.

Regards

DPB

0 Kudos
Reply
2,153 Views
ikkishingu
Contributor II

Hello DPB san,

Thank you! It makes sense to me!

Ikki

0 Kudos
Reply