Ipp and IOCD on S12ZVL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ipp and IOCD on S12ZVL

跳至解决方案
1,442 次查看
ikkishingu
Contributor II

Hello,

 

Let me just clarify.

There are specs about PP1,3 and 5 on S12ZVL RM rev1.01 Table A-9 #12&13

  Maximum allowed continuous current Ipp : -10 — +25 mA

  Over-current Detect Threshold IOCD : +40 — +80 mA

About these specs for sum of PP1,3 and 5? or for each port?

 

Best Regards,

Ikki

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,314 次查看
DPB
NXP Employee
NXP Employee

Hello Ikki

These specifications are valid for each individual pin.

However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.

Regards

DPB

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,315 次查看
DPB
NXP Employee
NXP Employee

Hello Ikki

These specifications are valid for each individual pin.

However please note that the specification is not valid for PP3 nor PP5 in package options without a VSSX2 pin.

Regards

DPB

0 项奖励
回复
1,314 次查看
ikkishingu
Contributor II

Hello DPB san,

Thank you! It makes sense to me!

Ikki

0 项奖励
回复