How to set parameters to reduce noise and vibration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set parameters to reduce noise and vibration

1,158 次查看
克年横井
Contributor I

Hello

I downloaded MC9S12ZVML128 PMSM Sensorless and turned my motor.

However, when turning the motor, noise and vibration have come out.
Motor parameters reflected the measured values.

Are there other parameters to adjust for turning the motor so as not to reduce or deteriorate the noise or vibration?
Also, please let me know if you have any precautions on reflecting parameters.

Best regards.

(Parameters listed are before change)

Parameter.png

0 项奖励
回复
2 回复数

982 次查看
pachamatej
NXP Employee
NXP Employee

Hello,

First of all, any noise or vibration is a very complex issue.

I would recommend to use the https://www.nxp.com/docs/en/application-note/AN4680.pdf  to determine as precise parameters as possible.

If it helps, then it is the easier situation. If not, I would recommend to lower the dynamics of the control to allow the controllers to act as "filters".

Matej

0 项奖励
回复

982 次查看
克年横井
Contributor I

Thank you for your reply.

I will check the contents of the application note.

Katsutoshi

0 项奖励
回复