How to set parameters to reduce noise and vibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set parameters to reduce noise and vibration

1,149件の閲覧回数
克年横井
Contributor I

Hello

I downloaded MC9S12ZVML128 PMSM Sensorless and turned my motor.

However, when turning the motor, noise and vibration have come out.
Motor parameters reflected the measured values.

Are there other parameters to adjust for turning the motor so as not to reduce or deteriorate the noise or vibration?
Also, please let me know if you have any precautions on reflecting parameters.

Best regards.

(Parameters listed are before change)

Parameter.png

0 件の賞賛
返信
2 返答(返信)

973件の閲覧回数
pachamatej
NXP Employee
NXP Employee

Hello,

First of all, any noise or vibration is a very complex issue.

I would recommend to use the https://www.nxp.com/docs/en/application-note/AN4680.pdf  to determine as precise parameters as possible.

If it helps, then it is the easier situation. If not, I would recommend to lower the dynamics of the control to allow the controllers to act as "filters".

Matej

0 件の賞賛
返信

973件の閲覧回数
克年横井
Contributor I

Thank you for your reply.

I will check the contents of the application note.

Katsutoshi

0 件の賞賛
返信