AMMCLIB errors in SWLIBS_MacroDisp.h

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AMMCLIB errors in SWLIBS_MacroDisp.h

1,102件の閲覧回数
xiemeijuan
Contributor II

When I using AMMCLIB in S12ZVM, issues as following in SWLIBS_MacroDisp.h

#ifndef SWLIBS_MACRODISP_H_
#define SWLIBS_MACRODISP_H_

#ifndef _MATLAB_BAM_CREATE
 /*
 * @violates @ref SWLIBS_MacroDisp_h_REF_1 MISRA 2004 Required Rule 19.4, Disallowed definition for 
 * macro. 
 * @violates @ref SWLIBS_MacroDisp_h_REF_2 MISRA 2004 Advisory Rule 19.7, Function-like macro 
 * defined. 
 * @violates @ref SWLIBS_MacroDisp_h_REF_3 MISRA 2004 Required Rule 20.2, Re-use of C90 identifier. 
 * @violates @ref SWLIBS_MacroDisp_h_REF_4 MISRA 2004 Required Rule 19.10, Unparenthesized macro 
 * parameter in definition of macro. 
 */
 #define _ARG2(_0, _1, _2, _3, _4, _5, _6, _7,...) _7       bad macro argument
 /*
 * @violates @ref SWLIBS_MacroDisp_h_REF_1 MISRA 2004 Required Rule 19.4, Disallowed definition for 
 * macro. 
 * @violates @ref SWLIBS_MacroDisp_h_REF_2 MISRA 2004 Advisory Rule 19.7, Function-like macro 
 * defined. 
 * @violates @ref SWLIBS_MacroDisp_h_REF_4 MISRA 2004 Required Rule 19.10, Unparenthesized macro 
 * parameter in definition of macro. 
 */
 #define VA_NUM_ARGS(...) _ARG2(__VA_ARGS__, 7, 6, 5, 4, 3, 2, 1, 0)bad macro argument  
 /*
 * @violates @ref SWLIBS_MacroDisp_h_REF_1 MISRA 2004 Required Rule 19.4, Disallowed definition for 
 * macro. 
 * @violates @ref SWLIBS_MacroDisp_h_REF_2 MISRA 2004 Advisory Rule 19.7, Function-like macro 
 * defined. 
 * @violates @ref SWLIBS_MacroDisp_h_REF_4 MISRA 2004 Required Rule 19.10, Unparenthesized macro 
 * parameter in definition of macro. 
 */
 #define macro_dispatcher(func, ...) macro_dispatcher_(func, VA_NUM_ARGS(__VA_ARGS__))
bad macro argument
/* * @violates @ref SWLIBS_MacroDisp_h_REF_1 MISRA 2004 Required Rule 19.4, Disallowed definition for * macro. * @violates @ref SWLIBS_MacroDisp_h_REF_2 MISRA 2004 Advisory Rule 19.7, Function-like macro * defined. * @violates @ref SWLIBS_MacroDisp_h_REF_4 MISRA 2004 Required Rule 19.10, Unparenthesized macro * parameter in definition of macro. */ #define macro_dispatcher_(func, nargs) macro_dispatcher__(func, nargs) #endif /* _MATLAB_BAM_CREATE */ /* * @violates @ref SWLIBS_MacroDisp_h_REF_1 MISRA 2004 Required Rule 19.4, Disallowed definition for * macro. * @violates @ref SWLIBS_MacroDisp_h_REF_2 MISRA 2004 Advisory Rule 19.7, Function-like macro * defined. * @violates @ref SWLIBS_MacroDisp_h_REF_5 MISRA 2004 Advisory Rule 19.13, #/##' operator used in * macro. * @violates @ref SWLIBS_MacroDisp_h_REF_6 MISRA 2004 Required Rule 19.12, Multiple use of '#/##' * operators in definition of macro. */ #define macro_dispatcher__(func, nargs) func##_Dsptchr_## nargs #endif /* SWLIBS_MACRODISP_H_ */

Three bad macro argument error information  in SWLIBS_MacroDisp.h. My compiler is cosmic.

The latest MC9S12ZVM_AMMCLIB_v1.1.12 is used. 

So anyone has encountered this problem before? I am looking forward your help. Thanks

0 件の賞賛
返信
0 返答(返信)