How to set parameters to reduce noise and vibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set parameters to reduce noise and vibration

1,197 Views
克年横井
Contributor I

Hello

I downloaded MC9S12ZVML128 PMSM Sensorless and turned my motor.

However, when turning the motor, noise and vibration have come out.
Motor parameters reflected the measured values.

Are there other parameters to adjust for turning the motor so as not to reduce or deteriorate the noise or vibration?
Also, please let me know if you have any precautions on reflecting parameters.

Best regards.

(Parameters listed are before change)

Parameter.png

0 Kudos
Reply
2 Replies

1,021 Views
pachamatej
NXP Employee
NXP Employee

Hello,

First of all, any noise or vibration is a very complex issue.

I would recommend to use the https://www.nxp.com/docs/en/application-note/AN4680.pdf  to determine as precise parameters as possible.

If it helps, then it is the easier situation. If not, I would recommend to lower the dynamics of the control to allow the controllers to act as "filters".

Matej

0 Kudos
Reply

1,021 Views
克年横井
Contributor I

Thank you for your reply.

I will check the contents of the application note.

Katsutoshi

0 Kudos
Reply