Debugger EEPROM-Read S12ZVML128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugger EEPROM-Read S12ZVML128

2,170 次查看
axel_hubner
Contributor I

Hi,

 

we are using PE-Micro Multilink Universal for Debugging in our development.

When we read the EEPROM in the memory-view in Codewarrior the first 72 bytes of the EERPOM will be returned as zero even when data is written into the memory area.

 

When we use the Onboard-Debugger of the S12ZVML12EVBLIN Eval-Board the EEPROM is returned correctly. For tests we use the BDM interface of the EVAL-Board and connect with a Multilink Universal Debugger and wrong data is read (0x00).

The Bus-clock is configured to 50 Mhz, the FCLKDIV to 0x31.

 

Are there any known bugs or special debugger settings necessary to read the EEPROM?

Eeprom_After_Erase_and_Program_Then_Connect.PNG

Regards


Axel

3 回复数

2,026 次查看
pbouten
Contributor II

I have the same issue as mentioned in Debugger EEPROM-Read S12ZVML128 since I use:

CodeWarrior for MCU
Version: 11.1
Build Id:181224

Never experienced the problem in previous versions.

0 项奖励
回复

2,026 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

ups, I see I ansewered something different previously.

I do not know, what could be wrong..I'll report it but you can use another option to view memory....

go to option:     Window->Show View -> Memory Browser

The difference address 0xFE0000:
pastedImage_1.png

The difference address 0x100000:

pastedImage_3.png

Best regards,

Ladislav

0 项奖励
回复

2,026 次查看
lama
NXP TechSupport
NXP TechSupport

Dear Axel Hubner, 

Yes, there is a rule which has to be met.
The flash or EEPROM block is not allowed to be read while the part of it is being erased or written. So, you are no allowed to have memory block in the window of the debugger when you step the code which performs E/W. (It causes flash process error)
There could be different timing of memory read action between OSBDM and Pemicro USB BDM which makes difference in processing and data visualization.I believe this is the reason.

Best regards,

Ladislav

0 项奖励
回复