Customising ISR of Watchdog Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Customising ISR of Watchdog Interrupt

4,156 次查看
santhoshsl
Contributor III

I am using mc9s12xdp512 controller for our project development.

As part of our development, we are now planning to have Diagnostics for our system.

So as part of this we want to capture and log Watchdog Reset.

 

For this I tried to write my own ISR or function and tried to assign this to vector table at 0xFFFA. But compiler gave error saying this Vector location is already assigned with System Reset point.

 

So can someone let me know, is there any way to capture and log failure that Watchdog reset has happened.

Or can you let me know how we can customize the ISR of watchdog?

标签 (1)
标记 (3)
9 回复数

3,340 次查看
tafengchung
Contributor II

Hi  Radek Sestak 

Do you have 9S12XEP 100  COP Reset Example?

0 项奖励
回复

3,340 次查看
RadekS
NXP Employee
NXP Employee

Hi Tafeng,

Sure, please see attached example codes. 

Please be aware that COP reset source detection may be affected by external capacitance at RESET pin. For more details, please look at:

S12 FAMILY DEVICES COP RECOGNITION CONSIDERATIONS_v2.0.pdf 

Other examples for S12XE:

S12X Examples Pack 

LAMA's S12XE unofficial examples 

I hope it helps you.

Have a great day,
Radek

3,339 次查看
tafengchung
Contributor II

Hi Sestak

Thnaks for your great support

0 项奖励
回复

3,339 次查看
RadekS
NXP Employee
NXP Employee

COP watchdog reset is hardware reset. It cannot be debugging via BDM because BDM communication/synchronization is lost during reset. I would like recommend simple LEDs for debugging watchdog reset.

In attachment you can find simple example code for COP watchdog.

You cannot handle this event as standard Interrupt. Standard Interrupt ends by RTI assembler command. COP reset interrupt routine must ending by jump to main program (there is no place where program can return).

I would like notice that code in COP_ISR runs before Start12.c code therefore variables and stack are not initialized. So, I would like to recommend use simplest code as possible.

External circuitry connected to the RESET pin should not include a large capacitance that would interfere with the ability of this signal to rise to a valid logic 1 within 64 SYSCLK cycles after the low drive is released. See chapter 2.5 Resets at S12XD RM(page 113).

For detecting COP reset it is necessary that voltage level at RESET pin achieve high level during 64 SYSCLK cycles after RESET pin release. After reset, SYSCLK value is equal to OSCCLK. If we take case when we use 16MHz oscillator, 64 SYSCLK cycles presents 4us.

So, if we have 2.2kOhm pull-up resistor at RESET pin, capacitance at RESET pin should be below approximately 1.8nF. Otherwise we detect POR / LVR / Illegal Address Reset / External Reset.

Note: Simply RC cell, RC constant=Tau=R*C represents time when voltage achieve approximately 2/3 value. Safety detection level for high value at pin is also approximately 2/3 value of VCC. So we can use simply calculation. C<64/(R*fOSC). In calculation we omitted capacitance and internal pull-up of RESET pin.

3,339 次查看
santhoshsl
Contributor III

Hello Radek,

Thanks for your elaborate inputs and sorry for my delay in reply.

I used the code sent by you by adding code to update COPCTL with some value and LED on.

I am using s12x DP512 evaluation board and i think it doesnot have higher capacitence. So there should be no issue with this to reset pin.

But with the project attached with this reply, i was not able to see the System Reset by COP and COP ISR execution.

Can you please help me with this.

0 项奖励
回复

3,340 次查看
RadekS
NXP Employee
NXP Employee

Which evaluation board you are using?

Evaluation board typically use 100nF capacitor at RESET pin (This too much for COP reset detection).

If you using SK-S12XDP512 (EVB9S12XDP512), please disassemble C213 (top side of PCB, near to CRYSTAL).

If you using DEMO9S12XDT512, please disassemble C36 (bottom side of PCB, near to RESET button).

If you using APS12XDT512(CSMB12XDT512), please disassemble C46 (bottom side of PCB, near to RESET button).

3,340 次查看
TICS_Fiona
NXP Employee
NXP Employee

Could you pleas check the PRM file, as well as the source code for interrupt vector? Whether address 0xFFFA is allocated twice?

Below is the code for COP vector in PE stationery, hope it helps! If not, could you please attach a simple project to help us reproduce the error?

static const tIsrFunc _ResetVectorTable[] @0xFFFAU = { /* Reset vector table */

/*lint -restore Enable MISRA rule (1.1) checking. */

  /* Reset handler name                    Address Name           Description */

  &_EntryPoint,                         /* 0xFFFA  ivVcop         unused by PE */

  &_EntryPoint,                         /* 0xFFFC  ivVclkmon      unused by PE */

  &_EntryPoint                          /* 0xFFFE  ivVreset       used by PE */

};

3,340 次查看
santhoshsl
Contributor III

Hello Fiona,,

Thanks for your inputs and sorry for delay in my reply.

I couldnot find the COP vector code you mentioned above. I searched in Startup.c and entire project. But couldnot find.

Attached is the project i am trying this with.

Can you please help me with this.

0 项奖励
回复

3,340 次查看
santhoshsl
Contributor III

Can someone help with this thing.

0 项奖励
回复