LS2085ARDB reflector example source code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS2085ARDB reflector example source code

跳至解决方案
1,797 次查看
lpapadop
Contributor I

I need to study the source files of the AIOP reflector example. The documentation (AIOP SDK Applications Debug Rev. 02/2016) suggests to download the files from http://linux.freescale.net/labDownload2/viewDownloads.php?Filter=LS2085A+Preliminary+SDK&field=PL&Ac.... However, this link is dead. Can you please provide the correct link?

Regards,

Lazaros

标记 (2)
0 项奖励
回复
1 解答
1,596 次查看
bpe
NXP Employee
NXP Employee

AIOP Reflector is part of LS2085 BSP Early Access Release. This package
is provided under NDA, there are no publicly available links.
Please contact your distributor or FAE for assistance in obtaining it.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,597 次查看
bpe
NXP Employee
NXP Employee

AIOP Reflector is part of LS2085 BSP Early Access Release. This package
is provided under NDA, there are no publicly available links.
Please contact your distributor or FAE for assistance in obtaining it.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复