LS2085ARDB reflector example source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2085ARDB reflector example source code

ソリューションへジャンプ
1,783件の閲覧回数
lpapadop
Contributor I

I need to study the source files of the AIOP reflector example. The documentation (AIOP SDK Applications Debug Rev. 02/2016) suggests to download the files from http://linux.freescale.net/labDownload2/viewDownloads.php?Filter=LS2085A+Preliminary+SDK&field=PL&Ac.... However, this link is dead. Can you please provide the correct link?

Regards,

Lazaros

タグ(2)
0 件の賞賛
返信
1 解決策
1,582件の閲覧回数
bpe
NXP Employee
NXP Employee

AIOP Reflector is part of LS2085 BSP Early Access Release. This package
is provided under NDA, there are no publicly available links.
Please contact your distributor or FAE for assistance in obtaining it.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,583件の閲覧回数
bpe
NXP Employee
NXP Employee

AIOP Reflector is part of LS2085 BSP Early Access Release. This package
is provided under NDA, there are no publicly available links.
Please contact your distributor or FAE for assistance in obtaining it.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信