LS2085ARDB reflector example source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2085ARDB reflector example source code

Jump to solution
1,818 Views
lpapadop
Contributor I

I need to study the source files of the AIOP reflector example. The documentation (AIOP SDK Applications Debug Rev. 02/2016) suggests to download the files from http://linux.freescale.net/labDownload2/viewDownloads.php?Filter=LS2085A+Preliminary+SDK&field=PL&Ac.... However, this link is dead. Can you please provide the correct link?

Regards,

Lazaros

Tags (2)
0 Kudos
Reply
1 Solution
1,617 Views
bpe
NXP Employee
NXP Employee

AIOP Reflector is part of LS2085 BSP Early Access Release. This package
is provided under NDA, there are no publicly available links.
Please contact your distributor or FAE for assistance in obtaining it.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,618 Views
bpe
NXP Employee
NXP Employee

AIOP Reflector is part of LS2085 BSP Early Access Release. This package
is provided under NDA, there are no publicly available links.
Please contact your distributor or FAE for assistance in obtaining it.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply