LS1021A ethernet interfaces (devel is the detail)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A ethernet interfaces (devel is the detail)

494 Views
ljbrits
Contributor I

According to the LS1021A datasheet and ref manual summary part, it is implied that all Ethernet controllers (1-3) support the RMII interface. But when you dig deeper into the register settings on P260-261 it seems that the LS1021 only supports 1x RMII port (the other two is MII) !? Is this correct?

1 Reply

418 Views
bpe
NXP Employee
NXP Employee

Yes, only eTSEC3 supports RMII on LS1021A. Note also that  eTSEC1/eTSEC2  MII is mutually exclusive with any eTSEC3 parallel interface due to signal multiplexing. See LS1021ARM, Table 3-13 for details.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------