Init_I2S error messages

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Init_I2S error messages

ソリューションへジャンプ
2,200件の閲覧回数
robotjosh
Contributor IV

I get errors when I try to use the I2S master clock in the Init_I2S bean.  When I set the serial master clock pin I get this error :

DescriptionResourcePathLocationType
Direction Output cannot be set. Supported directions are: [Input/Output] (Pin)Main_K22I2S0/PinProcessor Expert Problem

I've tried changing that pin to the other available master clock pin and get the same error.  If I make it an input instead of an output I get a similar error that "Direction Input cannot be set."

I attached a screenshot of the problem.i2s_error.png

タグ(1)
1 解決策
2,096件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Josh,

I have send you the method to your email , have you receive it ?

The Processor Expert team engineer saids :

"

- In the component inspector of the Init_I2S component, open the context menu of the Pin property in the Serial Master clock pin group and select "Enable Automatic". The selection of the pin is cleared and an error is repoted (no pin selected).

pastedImage_0.png
- Open Component Inspector of the PinSettings, select Collapsed View Mode, I2S tab and select the required pin in the I2S0 > MCLK - Master clock property. The pin is selected and properly routed and the selected pin is also displayed in the Pin property in the Init_I2S component.

pastedImage_1.png

"

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

元の投稿で解決策を見る

2 返答(返信)
2,097件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Josh,

I have send you the method to your email , have you receive it ?

The Processor Expert team engineer saids :

"

- In the component inspector of the Init_I2S component, open the context menu of the Pin property in the Serial Master clock pin group and select "Enable Automatic". The selection of the pin is cleared and an error is repoted (no pin selected).

pastedImage_0.png
- Open Component Inspector of the PinSettings, select Collapsed View Mode, I2S tab and select the required pin in the I2S0 > MCLK - Master clock property. The pin is selected and properly routed and the selected pin is also displayed in the Pin property in the Init_I2S component.

pastedImage_1.png

"

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

2,096件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Josh,

I will reply you on the CRM , i have create a SR for you , SR# 1-3731045071 , 。

And you will receive my message by your email .

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 件の賞賛
返信