How do I assign PDB Pulse-out signals to physical pins?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How do I assign PDB Pulse-out signals to physical pins?

跳至解决方案
1,264 次查看
GR8geek
Contributor II

My target is K20D72M Tower Board and I am using Code Warrior 10.4. Processor Expert PDB Peripheral Initialization component provides three Pulse-outs (0 thru 2). How can these be assigned to physical signals with individual rising/falling edge delays?

Thanks,

-Irwin

0 项奖励
回复
1 解答
1,031 次查看
Petr_H
NXP Employee
NXP Employee

Hi,

I don't think that this is  possible. These are just internal signals, according to the reference manual : "Individual PDB pulse-out signals control each CMP Sample/Window timing".

I suggest using TimerUnit_LDD or Init_FTM component for generation of timed signal.


best regards

Petr Hradsky

Processor Expert Support Team

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,032 次查看
Petr_H
NXP Employee
NXP Employee

Hi,

I don't think that this is  possible. These are just internal signals, according to the reference manual : "Individual PDB pulse-out signals control each CMP Sample/Window timing".

I suggest using TimerUnit_LDD or Init_FTM component for generation of timed signal.


best regards

Petr Hradsky

Processor Expert Support Team

0 项奖励
回复