How do I assign PDB Pulse-out signals to physical pins?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I assign PDB Pulse-out signals to physical pins?

Jump to solution
1,305 Views
GR8geek
Contributor II

My target is K20D72M Tower Board and I am using Code Warrior 10.4. Processor Expert PDB Peripheral Initialization component provides three Pulse-outs (0 thru 2). How can these be assigned to physical signals with individual rising/falling edge delays?

Thanks,

-Irwin

0 Kudos
Reply
1 Solution
1,072 Views
Petr_H
NXP Employee
NXP Employee

Hi,

I don't think that this is  possible. These are just internal signals, according to the reference manual : "Individual PDB pulse-out signals control each CMP Sample/Window timing".

I suggest using TimerUnit_LDD or Init_FTM component for generation of timed signal.


best regards

Petr Hradsky

Processor Expert Support Team

View solution in original post

0 Kudos
Reply
1 Reply
1,073 Views
Petr_H
NXP Employee
NXP Employee

Hi,

I don't think that this is  possible. These are just internal signals, according to the reference manual : "Individual PDB pulse-out signals control each CMP Sample/Window timing".

I suggest using TimerUnit_LDD or Init_FTM component for generation of timed signal.


best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply