CW 10.2. Kinetis K60N512. Adding Freescale USB Stack v4.0.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.2. Kinetis K60N512. Adding Freescale USB Stack v4.0.

Jump to solution
2,358 Views
LeoS
Contributor I

I'm working with CW 10.2 for Kinetis K60N512.
I have project created with Processor Expert. I want to add project based on "Freescale USB Stack v4.0" to this project. Or I can do opposite, add Processor Expert project to the "Freescale USB Stack v4.0" project.

 

Thank you

0 Kudos
Reply
1 Solution
2,084 Views
MVa
NXP Employee
NXP Employee

USB Stack v4.0. can be used in the Processor Expert project.

See "..\Documentation\USBPEXQSG.pdf" in your "Freescale USB Stack v4.0.0" installation directory for more information.

 

Best Regards
MVa

View solution in original post

0 Kudos
Reply
1 Reply
2,085 Views
MVa
NXP Employee
NXP Employee

USB Stack v4.0. can be used in the Processor Expert project.

See "..\Documentation\USBPEXQSG.pdf" in your "Freescale USB Stack v4.0.0" installation directory for more information.

 

Best Regards
MVa

0 Kudos
Reply