CW 10.2. Kinetis K60N512. Adding Freescale USB Stack v4.0.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.2. Kinetis K60N512. Adding Freescale USB Stack v4.0.

ソリューションへジャンプ
2,353件の閲覧回数
LeoS
Contributor I

I'm working with CW 10.2 for Kinetis K60N512.
I have project created with Processor Expert. I want to add project based on "Freescale USB Stack v4.0" to this project. Or I can do opposite, add Processor Expert project to the "Freescale USB Stack v4.0" project.

 

Thank you

0 件の賞賛
返信
1 解決策
2,079件の閲覧回数
MVa
NXP Employee
NXP Employee

USB Stack v4.0. can be used in the Processor Expert project.

See "..\Documentation\USBPEXQSG.pdf" in your "Freescale USB Stack v4.0.0" installation directory for more information.

 

Best Regards
MVa

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,080件の閲覧回数
MVa
NXP Employee
NXP Employee

USB Stack v4.0. can be used in the Processor Expert project.

See "..\Documentation\USBPEXQSG.pdf" in your "Freescale USB Stack v4.0.0" installation directory for more information.

 

Best Regards
MVa

0 件の賞賛
返信