CW 10.2. Kinetis K60N512. Adding Freescale USB Stack v4.0.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW 10.2. Kinetis K60N512. Adding Freescale USB Stack v4.0.

跳至解决方案
2,351 次查看
LeoS
Contributor I

I'm working with CW 10.2 for Kinetis K60N512.
I have project created with Processor Expert. I want to add project based on "Freescale USB Stack v4.0" to this project. Or I can do opposite, add Processor Expert project to the "Freescale USB Stack v4.0" project.

 

Thank you

0 项奖励
回复
1 解答
2,077 次查看
MVa
NXP Employee
NXP Employee

USB Stack v4.0. can be used in the Processor Expert project.

See "..\Documentation\USBPEXQSG.pdf" in your "Freescale USB Stack v4.0.0" installation directory for more information.

 

Best Regards
MVa

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,078 次查看
MVa
NXP Employee
NXP Employee

USB Stack v4.0. can be used in the Processor Expert project.

See "..\Documentation\USBPEXQSG.pdf" in your "Freescale USB Stack v4.0.0" installation directory for more information.

 

Best Regards
MVa

0 项奖励
回复