About s12ZVH clock configuration on CW10.6-PE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About s12ZVH clock configuration on CW10.6-PE

跳至解决方案
3,421 次查看
Fan_xy
Contributor III

Hello,

I configure the Bus clock 32 MHZ, use internal clock ,  S12ZVH128 chips. CW 10.6 -PE

pastedImage_0.png

There is no error when build , while ,when debug, it show this :

pastedImage_1.png

Where is wrong ?

Thank you !

0 项奖励
回复
1 解答
3,143 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

I recieved feedback from P&E.

See below:

+++++++++++++++++++++++

OSBDM interface supports run control debug with devices operating at bus frequencies between 500khz and 24Mhz.

Hence, it will not be able to support talking to a device operating at 30Mhz bus frequency.

For debugging device operating at higher bus frequency rates, we recommend looking into using P&E's USB Universal Multilink hardware interface:

          http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137&menu_id=details

+++++++++++++++++++++++

Pascal

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,144 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

I recieved feedback from P&E.

See below:

+++++++++++++++++++++++

OSBDM interface supports run control debug with devices operating at bus frequencies between 500khz and 24Mhz.

Hence, it will not be able to support talking to a device operating at 30Mhz bus frequency.

For debugging device operating at higher bus frequency rates, we recommend looking into using P&E's USB Universal Multilink hardware interface:

          http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137&menu_id=details

+++++++++++++++++++++++

Pascal

0 项奖励
回复
3,143 次查看
marek_neuzil
NXP Employee
NXP Employee

Hi Pascal,

Thank you for the resolution of this issue.

Best Regards,

Marek Neuzil

0 项奖励
回复
3,143 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello,

The crash of the application can be caused by many reasons (debugger settings, error in a driver/application code, target board/silicon connection and so on).  Have you analyzed the application which part of the code (line) cause the error?

What target board and silicon are you using?

Could you send me the application for analysis, please?

Best Regards,

Marek Neuzil

0 项奖励
回复
3,141 次查看
trytohelp
NXP Employee
NXP Employee


Hi Marek,

I've reproduced the problem on my side too with a S12ZVML-MINIBRD.

I've reported the issue to P&E.

Attached a video showing the problem.

Pascal

0 项奖励
回复