About s12ZVH clock configuration on CW10.6-PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About s12ZVH clock configuration on CW10.6-PE

ソリューションへジャンプ
2,419件の閲覧回数
Fan_xy
Contributor III

Hello,

I configure the Bus clock 32 MHZ, use internal clock ,  S12ZVH128 chips. CW 10.6 -PE

pastedImage_0.png

There is no error when build , while ,when debug, it show this :

pastedImage_1.png

Where is wrong ?

Thank you !

0 件の賞賛
返信
1 解決策
2,141件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I recieved feedback from P&E.

See below:

+++++++++++++++++++++++

OSBDM interface supports run control debug with devices operating at bus frequencies between 500khz and 24Mhz.

Hence, it will not be able to support talking to a device operating at 30Mhz bus frequency.

For debugging device operating at higher bus frequency rates, we recommend looking into using P&E's USB Universal Multilink hardware interface:

          http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137&menu_id=details

+++++++++++++++++++++++

Pascal

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,142件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I recieved feedback from P&E.

See below:

+++++++++++++++++++++++

OSBDM interface supports run control debug with devices operating at bus frequencies between 500khz and 24Mhz.

Hence, it will not be able to support talking to a device operating at 30Mhz bus frequency.

For debugging device operating at higher bus frequency rates, we recommend looking into using P&E's USB Universal Multilink hardware interface:

          http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137&menu_id=details

+++++++++++++++++++++++

Pascal

0 件の賞賛
返信
2,141件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi Pascal,

Thank you for the resolution of this issue.

Best Regards,

Marek Neuzil

0 件の賞賛
返信
2,141件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

The crash of the application can be caused by many reasons (debugger settings, error in a driver/application code, target board/silicon connection and so on).  Have you analyzed the application which part of the code (line) cause the error?

What target board and silicon are you using?

Could you send me the application for analysis, please?

Best Regards,

Marek Neuzil

0 件の賞賛
返信
2,139件の閲覧回数
trytohelp
NXP Employee
NXP Employee


Hi Marek,

I've reproduced the problem on my side too with a S12ZVML-MINIBRD.

I've reported the issue to P&E.

Attached a video showing the problem.

Pascal

0 件の賞賛
返信