About s12ZVH clock configuration on CW10.6-PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About s12ZVH clock configuration on CW10.6-PE

Jump to solution
2,415 Views
Fan_xy
Contributor III

Hello,

I configure the Bus clock 32 MHZ, use internal clock ,  S12ZVH128 chips. CW 10.6 -PE

pastedImage_0.png

There is no error when build , while ,when debug, it show this :

pastedImage_1.png

Where is wrong ?

Thank you !

0 Kudos
Reply
1 Solution
2,137 Views
trytohelp
NXP Employee
NXP Employee

Hi,

I recieved feedback from P&E.

See below:

+++++++++++++++++++++++

OSBDM interface supports run control debug with devices operating at bus frequencies between 500khz and 24Mhz.

Hence, it will not be able to support talking to a device operating at 30Mhz bus frequency.

For debugging device operating at higher bus frequency rates, we recommend looking into using P&E's USB Universal Multilink hardware interface:

          http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137&menu_id=details

+++++++++++++++++++++++

Pascal

View solution in original post

0 Kudos
Reply
4 Replies
2,138 Views
trytohelp
NXP Employee
NXP Employee

Hi,

I recieved feedback from P&E.

See below:

+++++++++++++++++++++++

OSBDM interface supports run control debug with devices operating at bus frequencies between 500khz and 24Mhz.

Hence, it will not be able to support talking to a device operating at 30Mhz bus frequency.

For debugging device operating at higher bus frequency rates, we recommend looking into using P&E's USB Universal Multilink hardware interface:

          http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137&menu_id=details

+++++++++++++++++++++++

Pascal

0 Kudos
Reply
2,137 Views
marek_neuzil
NXP Employee
NXP Employee

Hi Pascal,

Thank you for the resolution of this issue.

Best Regards,

Marek Neuzil

0 Kudos
Reply
2,137 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

The crash of the application can be caused by many reasons (debugger settings, error in a driver/application code, target board/silicon connection and so on).  Have you analyzed the application which part of the code (line) cause the error?

What target board and silicon are you using?

Could you send me the application for analysis, please?

Best Regards,

Marek Neuzil

0 Kudos
Reply
2,135 Views
trytohelp
NXP Employee
NXP Employee


Hi Marek,

I've reproduced the problem on my side too with a S12ZVML-MINIBRD.

I've reported the issue to P&E.

Attached a video showing the problem.

Pascal

0 Kudos
Reply