local memory Map for MPC8358E processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

local memory Map for MPC8358E processor

ソリューションへジャンプ
16,304件の閲覧回数
venkat1
Contributor III

Hi Folks

We are using MPC8358E processor and we configured the local memory as shown in the fig.. mainly we are struggling with DDR interface. so please confirm this memory mapping.

is this DDR memory mapping is right?

venkat1_1-1602481094362.pngvenkat1_1-1602481094362.png

Regards,

Venkat

ラベル(1)
  • DDR

0 件の賞賛
返信
1 解決策
16,196件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual, 4.4.3 System Clock Domains:

"The internal ddr_clk frequency (for DDR) is determined by RCWL[DDRCM]. Note that the lb_clk clock
frequency (for Secondary DDR) is determined by RCWL[LBCM]. See Section 4.3.2.1, “Reset
Configuration Word Low Register (RCWLR).” Note that ddr_clk is not the external memory bus
frequency; ddr_clk passes through the DDR clock divider (÷2) to create the differential DDR memory bus
clock outputs (MCK and MCK). However, the data rate is the same frequency as ddr_clk."

元の投稿で解決策を見る

0 件の賞賛
返信
18 返答(返信)
16,297件の閲覧回数
ufedor
NXP Employee
NXP Employee

Proposed memory map is incorrect.

Please read the MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual, 5.2 Local Memory Map Overview and Example

0 件の賞賛
返信
16,293件の閲覧回数
venkat1
Contributor III

Thank you for replying,

As per MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual says, we can put  boot flash on All zeros address or 0xFF80_0000 address. can you please elaborate more on this?.  so that, my memory mapping is incorrect...

Regards,

Venkat

0 件の賞賛
返信
16,288件の閲覧回数
ufedor
NXP Employee
NXP Employee

What is the DDR SDRAM size?

0 件の賞賛
返信
16,283件の閲覧回数
venkat1
Contributor III

DDR size-64MB

Manfr- micron

0 件の賞賛
返信
16,275件の閲覧回数
ufedor
NXP Employee
NXP Employee

What are RCWLR and RCWHR values?

 

 You wrote:

> we are struggling with DDR interface

What does it mean?

0 件の賞賛
返信
16,268件の閲覧回数
venkat1
Contributor III

RCWLR- 0x02230086

RCWHR- 0x00600000

 

0 件の賞賛
返信
16,262件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:

> we are struggling with DDR interface

What does it mean?

0 件の賞賛
返信
16,253件の閲覧回数
venkat1
Contributor III

 

#RCWLR Value :- 0x02230086

#LBCM-0   LBCM is equal to csb clk (266MHz)

#DDRCM-0  DDRCM is equal to csb clk (266MHz)

#SVCOD-00  system PLL VCO division is 4

#SPMF - 0010 system PLL multiplication factor is 2:1

#COREPLL -0100011 Core freq.  1600MHZ 

#CEVCOD -10 QUIIC engine Freq. is 800MHZ

#CEPDF - 0  QUIIC Engine PLL div. factor is 0

#CEPMF- 00110 QUICC engine PLL mortification factor 6

 

#RCWHR Value :- 0x00600000

#PCIHOST-0   PCI is disable (not using)

#PCIARB-0  PCI arbiter is disable

#PCICKDRV - 0 PCI Buffers are disable

#COEDIS- 0 core can boot without waiting for config. by external master

#BMS- 0 boot memory space is all zeros to 0x007f_ffff

#BOOTSEQ- 00 boot sequencer disabled

#SWEN - 0 Software WDT disable

#ROMLOC- 110 local bus GPCM 16-bit ROM

#SDDRIOE -0 secondary DDR I/O disable

#TLE -0 big-endian mode

#LALE - 0 normal LALE timing 

#LDP-0 initial value  of SCIRL[LDP_A] is 1 means that LDP0-LDP3 are used for local data parity

 

 

 

0 件の賞賛
返信
16,250件の閲覧回数
venkat1
Contributor III

And please find the attached document of my init file 

0 件の賞賛
返信
16,242件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:

> we are struggling with DDR interface

What does it mean?

0 件の賞賛
返信
16,239件の閲覧回数
venkat1
Contributor III

> we are struggling with DDR interface

>What does it mean?

I am not able to access DDR memory. and DDR doesn't  responding to the configured address. 

 

0 件の賞賛
返信
16,237件の閲覧回数
ufedor
NXP Employee
NXP Employee

There are two possibilities:

1) DDR SDRAM connection is incorrect

2) DDR controller initialization settings are incorrect.

0 件の賞賛
返信
16,232件の閲覧回数
venkat1
Contributor III

There is no doubt in DDR SDRAM hardware part.

I am not sure about DDR controller initialization settings..

PFA of DDR controller initialization file 

0 件の賞賛
返信
16,215件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide:

1) DDR SDRAM connection schematics as searchable PDF

2) what is measured frequency of the MCK?

0 件の賞賛
返信
16,205件の閲覧回数
venkat1
Contributor III

PFA of DDR SDRAM interface Schematic

&

MCK frequency is 133MHZ

0 件の賞賛
返信
16,219件の閲覧回数
venkat1
Contributor III

@ufedor  are u there?

0 件の賞賛
返信
16,203件の閲覧回数
venkat1
Contributor III

sir,

can we control DDR  operating frequecy(MCK)? if it is yes!  How?

 

 

0 件の賞賛
返信
16,197件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual, 4.4.3 System Clock Domains:

"The internal ddr_clk frequency (for DDR) is determined by RCWL[DDRCM]. Note that the lb_clk clock
frequency (for Secondary DDR) is determined by RCWL[LBCM]. See Section 4.3.2.1, “Reset
Configuration Word Low Register (RCWLR).” Note that ddr_clk is not the external memory bus
frequency; ddr_clk passes through the DDR clock divider (÷2) to create the differential DDR memory bus
clock outputs (MCK and MCK). However, the data rate is the same frequency as ddr_clk."

0 件の賞賛
返信