T4240_PCIE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240_PCIE

5,395件の閲覧回数
jeffcao
Contributor I

I designed the circuit on the T4240 chip through the PCIE connected to the bridge(PCIE-SATA ), but at low temperatures through the PCIE can not recognize the bridge.

What is the maximum length of chip(T4240) support in PCIE2.0?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

5,221件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached files. These files contain recommendations for PCI layout and information about maximum length.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,221件の閲覧回数
jeffcao
Contributor I

Hi pavel

In attached files,I dont find about  PCI layout and design guide

Thankyou 

0 件の賞賛
返信