MPC886 tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,529件の閲覧回数
cathy363
Contributor I

Hi,

For MPC886, which kinds of tool can help to program?

I saw "USBTAP_PQ1: USB TAP for PowerQUICC® I" can support MPC885. (USB TAP for PowerQUICC® I|NXP )

Is it also can support MPC886??

Thank you.

Regards,

Cathy

0 件の賞賛
返信
1 解決策
1,469件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, USB TAP for PowerQuicc1 processors may be used for all processors from this family - all MPC8xx parts, including MPC866.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,470件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, USB TAP for PowerQuicc1 processors may be used for all processors from this family - all MPC8xx parts, including MPC866.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------