MPC886 tool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC886 tool?

跳至解决方案
1,523 次查看
cathy363
Contributor I

Hi,

For MPC886, which kinds of tool can help to program?

I saw "USBTAP_PQ1: USB TAP for PowerQUICC® I" can support MPC885. (USB TAP for PowerQUICC® I|NXP )

Is it also can support MPC886??

Thank you.

Regards,

Cathy

0 项奖励
回复
1 解答
1,463 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, USB TAP for PowerQuicc1 processors may be used for all processors from this family - all MPC8xx parts, including MPC866.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,464 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, USB TAP for PowerQuicc1 processors may be used for all processors from this family - all MPC8xx parts, including MPC866.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------