MPC886 tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC886 tool?

Jump to solution
983 Views
cathy363
Contributor I

Hi,

For MPC886, which kinds of tool can help to program?

I saw "USBTAP_PQ1: USB TAP for PowerQUICC® I" can support MPC885. (USB TAP for PowerQUICC® I|NXP )

Is it also can support MPC886??

Thank you.

Regards,

Cathy

0 Kudos
Reply
1 Solution
923 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, USB TAP for PowerQuicc1 processors may be used for all processors from this family - all MPC8xx parts, including MPC866.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
924 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, USB TAP for PowerQuicc1 processors may be used for all processors from this family - all MPC8xx parts, including MPC866.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------