VR5510 Bandgap voltage specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VR5510 Bandgap voltage specification

Jump to solution
3,840 Views
K_Steinhammer
Contributor III

In an application with functional safety requirements, we need an independent reference voltage for periodically testing the ADC of the CPU.

Now there is the idea to measure one bandgap voltage of the VR5510 PMIC via the AMUX pin for reference. Unfortunately the bandgap voltage specifications are missing in the datasheet.

Is there a document with the missing specifications (voltage and accuracy of Bandgap Main and Bandgap Fail-safe)?

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,642 Views
K_Steinhammer
Contributor III

Maybe this information is not available to the public - I got an answer within 24h after opening a support ticket (I have an active NDA).

So I advice anybody needing this information to do the same.

Thanks

View solution in original post

0 Kudos
Reply
3 Replies
3,643 Views
K_Steinhammer
Contributor III

Maybe this information is not available to the public - I got an answer within 24h after opening a support ticket (I have an active NDA).

So I advice anybody needing this information to do the same.

Thanks

0 Kudos
Reply
3,827 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please help and fill below :

1: customer name/location

2: end product/

3:schedule

4: volume/annual

0 Kudos
Reply
3,817 Views
K_Steinhammer
Contributor III

Requested information is sent via a PM.

 

Thanks

0 Kudos
Reply