VR5510 Bandgap voltage specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VR5510 Bandgap voltage specification

ソリューションへジャンプ
3,842件の閲覧回数
K_Steinhammer
Contributor III

In an application with functional safety requirements, we need an independent reference voltage for periodically testing the ADC of the CPU.

Now there is the idea to measure one bandgap voltage of the VR5510 PMIC via the AMUX pin for reference. Unfortunately the bandgap voltage specifications are missing in the datasheet.

Is there a document with the missing specifications (voltage and accuracy of Bandgap Main and Bandgap Fail-safe)?

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,644件の閲覧回数
K_Steinhammer
Contributor III

Maybe this information is not available to the public - I got an answer within 24h after opening a support ticket (I have an active NDA).

So I advice anybody needing this information to do the same.

Thanks

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,645件の閲覧回数
K_Steinhammer
Contributor III

Maybe this information is not available to the public - I got an answer within 24h after opening a support ticket (I have an active NDA).

So I advice anybody needing this information to do the same.

Thanks

0 件の賞賛
返信
3,829件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please help and fill below :

1: customer name/location

2: end product/

3:schedule

4: volume/annual

0 件の賞賛
返信
3,819件の閲覧回数
K_Steinhammer
Contributor III

Requested information is sent via a PM.

 

Thanks

0 件の賞賛
返信