Reference design for RT117x + MPF5020CMMACES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reference design for RT117x + MPF5020CMMACES

4,553 Views
mastupristi
Senior Contributor II

We are developing a board with RT1175 and MPF5020CMMACES.

Where can I find a reference design schematic, or some docs?

Please note that I read AN13213, but there is only the PMIC portion of the schematic there, I also need the reference design for RT1175.

I am convinced that NXP had to develop a board to test MPF5020 with RT117x. I wish I could see the schematics of that board.

 

best regards

Max

Labels (1)
0 Kudos
Reply
3 Replies

4,535 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Massimiliano,

please find a schematic of the RT1176 + PF5020 attached.

With Best Regards,

Jozef

0 Kudos
Reply

4,531 Views
mastupristi
Senior Contributor II

Thank you, this is really helpful to me.

 

Is this board also available for purchase?

 

best regards

0 Kudos
Reply

4,520 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Massimiliano,

yes, there is the board available. But not the rev. A, to which I have shared the schematic, but a newer rev. C1. The board name is: MIMXRT1170-EVKB. Please refer to the Revision History in the SPF-55139_c1 schematic attached.

JozefKozon_1-1681383204961.png

JozefKozon_0-1681383162851.png

With Best Regards,

Jozef

0 Kudos
Reply