RESET AND WATCHDOG PARAMETERS - FS6500

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RESET AND WATCHDOG PARAMETERS - FS6500

ソリューションへジャンプ
2,595件の閲覧回数
AnneVilasini
Contributor I

Hi , 

What is the maximum time taken for a reset to occur when a fault has occured? (indicated by Trr in the picture below)?

AnneVilasini_0-1606968849523.png

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,587件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

There is some misunderstanding for the reaction time and  Trr. To make clear, I will describe the total process for a fault happen and Reset assertion:

1. Recognition time

When output voltage reach UV threshold, and the duration time of output<UV Threshold larger than 10uS(max value),UV event will be recognized. It is 234us for an overvoltage recognition.

2. Internal Processing Time

After an fault recognized, it will take some time for internal Processing, the longest time is about 80 μs for an overvoltage detection. All others are below 80 μs.

3. External indication time 

External indication time to notify an observer about the failure external to the SBC. This time is 3.0 µs for RSTB, 22 μs for FS0B .

 

so,

It should be 10uS+80uS+3uS=93uS(max) from an undervoltage happen to RSTB asserted to Low;

it should be 234uS+80uS+3uS=317uS(max) from an overvoltage happen to RSTB asserted to Low; 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,588件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

There is some misunderstanding for the reaction time and  Trr. To make clear, I will describe the total process for a fault happen and Reset assertion:

1. Recognition time

When output voltage reach UV threshold, and the duration time of output<UV Threshold larger than 10uS(max value),UV event will be recognized. It is 234us for an overvoltage recognition.

2. Internal Processing Time

After an fault recognized, it will take some time for internal Processing, the longest time is about 80 μs for an overvoltage detection. All others are below 80 μs.

3. External indication time 

External indication time to notify an observer about the failure external to the SBC. This time is 3.0 µs for RSTB, 22 μs for FS0B .

 

so,

It should be 10uS+80uS+3uS=93uS(max) from an undervoltage happen to RSTB asserted to Low;

it should be 234uS+80uS+3uS=317uS(max) from an overvoltage happen to RSTB asserted to Low; 

 

0 件の賞賛
返信