Hi Jozef,
Thank you so much for your inputs, please advise the below:
1.If ON pin is always low, the device will reset every 4, 8, 12 or 16s(default 8s) for a long press duration time.
[SB] Please advise if there is any way to disable this feature?
2. BIT4 in I2C address is MTP option, this bit can be trim to 1 in the product line in the factory before chips go to customer side. MTP configured chips are special ordered compared default state chips.
[SB] in case the customer already ordered samples and plans for assembly in two weeks frame time, could you please advise if there is any workaround that can be done in order to change the BIT4?
or alternative how I can order as fast as possible 10 pcs with BIT4 trimmed to '1'?
I'll appreciate your fast responses, Thanks in advance.
Best Regards,
Shai