FS6510 Reading BIST Result needs a delay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS6510 Reading BIST Result needs a delay

ソリューションへジャンプ
4,024件の閲覧回数
Jamber_H
Contributor III

Hi, 

I read the BIST Register after power-on reset, the result is 0x0, it means all the 4 bits of BIST reault are NOTOK. But after a 8ms delay, I read this register again, it returns 0xD, it means ABIST2_VAUX is NOTOK, and other bits such as LBIST, ABIST1, ABIST2_FS1B are Normal. Why does it need a delay, what's the possible reason about it?

BIST延时.png

Best Regards,

Jamber

0 件の賞賛
返信
1 解決策
4,013件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jamber,

the 8ms is actually quite short delay time. According to the datasheet, the Reset delay time after a power on reset is typically 16.5ms, minimally 12.5ms. Please refer to the Table 6. in the datasheet attached.

JozefKozon_0-1626871580793.png

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,014件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jamber,

the 8ms is actually quite short delay time. According to the datasheet, the Reset delay time after a power on reset is typically 16.5ms, minimally 12.5ms. Please refer to the Table 6. in the datasheet attached.

JozefKozon_0-1626871580793.png

With Best Regards,

Jozef

0 件の賞賛
返信