FS6510 Reading BIST Result needs a delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6510 Reading BIST Result needs a delay

Jump to solution
4,015 Views
Jamber_H
Contributor III

Hi, 

I read the BIST Register after power-on reset, the result is 0x0, it means all the 4 bits of BIST reault are NOTOK. But after a 8ms delay, I read this register again, it returns 0xD, it means ABIST2_VAUX is NOTOK, and other bits such as LBIST, ABIST1, ABIST2_FS1B are Normal. Why does it need a delay, what's the possible reason about it?

BIST延时.png

Best Regards,

Jamber

0 Kudos
Reply
1 Solution
4,004 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jamber,

the 8ms is actually quite short delay time. According to the datasheet, the Reset delay time after a power on reset is typically 16.5ms, minimally 12.5ms. Please refer to the Table 6. in the datasheet attached.

JozefKozon_0-1626871580793.png

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
1 Reply
4,005 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jamber,

the 8ms is actually quite short delay time. According to the datasheet, the Reset delay time after a power on reset is typically 16.5ms, minimally 12.5ms. Please refer to the Table 6. in the datasheet attached.

JozefKozon_0-1626871580793.png

With Best Regards,

Jozef

0 Kudos
Reply